imx6q wpa_supplicant error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q wpa_supplicant error

1,721 次查看
推土机
Contributor II

I have a  AR6302 chip connected with sdio to my imx6q board.

I do as follows:

$ insmod ath6kl.ko

$ ifconfig wlan0 up

$ iwlist wlan0 scan

All above is ok.

Then I tried to connect to the wifi AP.

$ wpa_supplicant -Dwext -iwlan0 -c /etc/wpa_supplicant.conf

ioctl[SIOCSIWAUTH]: Operation not supported                                    

WEXT auth param 4 value 0x0 - Trying to associate with d0:c7:c0:a7:55:da (SSID=)

ioctl[SIOCSIWFREQ]: Operation not supported                                    

Association request to the driver failed   

Then i kill  wpa_supplicant and rerun the program.

$ wpa_supplicant -Dwext -iwlan0 -c /etc/wpa_supplicant.conf

Now it seems ok.

octl[SIOCSIWAUTH]: Operation not supported                                    

WEXT auth param 4 value 0x0 - Associated with d0:c7:c0:a7:55:da                

WPA: Key negotiation completed with d0:c7:c0:a7:55:da [PTK=CCMP GTK=CCMP]      

CTRL-EVENT-CONNECTED - Connection to d0:c7:c0:a7:55:da completed (auth) [id=0 i]

Then it can ping other machines successfully.

But sometimes the kernel output errors:

ath6kl: aggr timeout (st 143 end 174)                                          

And the system will hang for about 1 seconds.

I tried to send some video data:

gst-launch  -v tvsrc  device=/dev/video1  ! 'video/x-raw-yuv,format=(fourcc)UYVY,width=720,height=576,framerate=25/1' ! mfw_ipucsc ! 'video/x-raw-yuv,format=(fourcc)I420, width=720,height=576,framerate=25/1' ! vpuenc codec=avc ! video/x-h264,width=720,height=576 ! rtph264pay ! udpsink host=192.168.1.86 port=5004 sync=false async=false

The kernel crashs:

ath6kl: req failed (status:-110, ep:2, len:80 creds:1)                         

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:80 creds:1)                         

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:236 creds:1)                        

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:80 creds:1)                         

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:236 creds:1)                        

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:1484 creds:1)                       

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:1484 creds:1)                       

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:1484 creds:1)                       

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:1484 creds:1)                       

ath6kl: tx error, status: 0xffffff92                                           

ath6kl: req failed (status:-110, ep:2, len:1484 creds:1)                       

ath6kl: tx error, status: 0xffffff92                                           

------------[ cut here ]------------                                           

WARNING: at drivers/net/wireless/ath/ath6kl/sdio.c:499 sdio_irq_thread+0x1d4/0x)

Modules linked in: tvp5150_camera ath6kl                                       

[<800468e0>] (unwind_backtrace+0x0/0xf8) from [<800700dc>] (warn_slowpath_commo)

[<800700dc>] (warn_slowpath_common+0x4c/0x64) from [<80070110>] (warn_slowpath_)

[<80070110>] (warn_slowpath_null+0x1c/0x24) from [<80368148>] (sdio_irq_thread+)

[<80368148>] (sdio_irq_thread+0x1d4/0x2ac) from [<80089edc>] (kthread+0x80/0x88)

[<80089edc>] (kthread+0x80/0x88) from [<800400e4>] (kernel_thread_exit+0x0/0x8)

---[ end trace eca840746d727b64 ]---                                           

Seems I lost some kernel configuration options?

标签 (2)
0 项奖励
回复
2 回复数

1,303 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Which BSP are you using?

How did you add the AR6302 support and the corresponding firmware?

/Alejandro

0 项奖励
回复

1,303 次查看
推土机
Contributor II

BSP version is L3.0.35_4.1.0_130816.

Firmware got from BSP linux kernel source firmware/ath6kl.

-------

Later i tried compat wireless(https://wireless.wiki.kernel.org/en/users/download  backports-4.0.1-1.tar.gz) and firmware from BSP(L3.0.35_4.1.0_130816 kernel).

Now all seems ok. But the network is always delayed for about 0.5~1 second.

Seems problem with the firmware. Where could I got the right version firmware?

Thank you.

0 项奖励
回复