imx6q use ksz8863rll switch

cancel
Showing results for 
Search instead for 
Did you mean: 

imx6q use ksz8863rll switch

Jump to solution
1,982 Views
wenmintang
Contributor I

I use ksz8863rll on my board using RMII. My board is similar with imx6q_sabresd only using  10/100M switch instead of GRMII.  I have changed some code accroding OTT TV .

Now it can run, but when I insert only net1 wire it can work ok.the display is  as folw:

root@freescale ~$ PHY: 1:01 - Link is Up - 100/Full

but  I insert only net2 wire it cann't work.

it seems net1 port is master and net2 is slave.

why?

0 Kudos
1 Solution
202 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For the switch chip, it has one uplink port and two down link port, one of the down link port is connected to iMX6 fec directly, you can connect the uplink port to internet and connect a PC to another down link port, then both the PC and iMX6 board can access internet from the uplink port. This is the use case for this chip.

By the way, there is no KSZ8863 driver in uboot, if you want to enable it, you need porting the driver.

View solution in original post

0 Kudos
6 Replies
203 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

For the switch chip, it has one uplink port and two down link port, one of the down link port is connected to iMX6 fec directly, you can connect the uplink port to internet and connect a PC to another down link port, then both the PC and iMX6 board can access internet from the uplink port. This is the use case for this chip.

By the way, there is no KSZ8863 driver in uboot, if you want to enable it, you need porting the driver.

View solution in original post

0 Kudos
202 Views
wenmintang
Contributor I

if no ksz8863 drvier in uboot,ott cannot use ethernet in uboot?

0 Kudos
202 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Yes, because it is a switch chip, not a phy. It needs special driver.

0 Kudos
202 Views
wenmintang
Contributor I

I write a switch driver in uboot ,but when ping it cannot pass. and mdc clock is 2.5MHZ, GPIO_16 is 50MHZ.

MX6Q SABRESD U-Boot > ping 192.168.0.147

FEC: Link is Up 780c

10Mbps

=====

ievent       2188004 - 0

imask        2188008 - 0

r_des_active 2188010 - 1000000

x_des_active 2188014 - 0

ecntrl       2188024 - f0000102

mii_mframe   2188040 - 61fe0000

mii_speed    2188044 - 1a

mii_ctrlstat 2188064 - c0000000

r_cntrl      2188084 - 5ee0306

x_cntrl      21880c4 - 0

padr_l       21880e4 - 12345678

padr_u       21880e8 - 9abc8808

op_pause     21880ec - 10000

iadr_u       2188118 - 0

iadr_l       218811c - 0

gadr_u       2188120 - 0

gadr_l       2188124 - 0

x_wmrk       2188144 - 100

r_bound      218814c - 600

r_fstart     2188150 - 500

r_drng       2188180 - 27602d20

x_drng       2188184 - 27602d60

r_bufsz      2188188 - 5f0

Using FEC0 device

TX timeout packet at 2782b2c0

mxc_fec.c[618] fec_send: cycles: 50000    status: 8c00  retry cnt: 0

TX timeout packet at 2782b2c0

mxc_fec.c[618] fec_send: cycles: 50000    status: ac00  retry cnt: 0

TX not ready

TX timeout packet at 2782b2c0

mxc_fec.c[618] fec_send: cycles: 50000    status: 8c00  retry cnt: 0

TX not ready

0 Kudos
202 Views
gusarambula
NXP TechSupport
NXP TechSupport

That's correct. You would need a driver for the switch which is handling the PHYs.

0 Kudos
202 Views
wenmintang
Contributor I

Oh,My god!  It's diffcult for me!

0 Kudos