imx6q support lvds in android6.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q support lvds in android6.0

1,087 Views
jiejia
Contributor III

Dear all,

I have a board reference imx6q sabresd. I have a lvds display panel with 1280x800 resolution connected to LVDS0.

I have downloaded the android_M6.0.1_2.0.0_image_6dqpsabresd.tar.gz files to my board.

I want to make this lvds display panel works well.  Do I need to change linux kernel source or device trees? What should the bootargs is?

0 Kudos
Reply
1 Reply

721 Views
BiyongSUN
NXP Employee
NXP Employee

You need to change the display timing according the display panel spec.

The Linux binding guide for dts document could be found in the Documentation\devicetree\bindings\video\display-timing.txt

0 Kudos
Reply