imx6q ro.sf.hwrotation issue (android 7.1)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q ro.sf.hwrotation issue (android 7.1)

1,894 Views
jiujinhong
Contributor IV

Hi, we support Portrait mode through  "set ro.sf.hwrotation 270 in init.rc" for our display/mechnical limit. But sometimes bootanimation become landscape mode  before launcher start. can you give some advice for it? 

Labels (2)
0 Kudos
1 Reply

1,520 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiu

 rotation should be implemented in graphics manager middleware, such as X11

and Android SurfaceFlinger, one can check suggestions on

Default display orientation in Android 8 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos