my linux L3.0.35_Version is 1.1.0_121218,MSI does not work in the version but I Want use pcie,this is my dmesg:
root@freescale ~$ dmesg
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
imx-i2c imx-i2c.1: <i2c_imx_probe>
imx-i2c imx-i2c.1: <i2c_imx_probe> bitrate:100000
mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
i2c i2c-1: claimed irq 69
i2c i2c-1: device resources from 0x21a4000 to 0x21a4fff
i2c i2c-1: allocated 4096 bytes at 0x21a4000
i2c i2c-1: adapter name: "imx-i2c"
i2c i2c-1: IMX I2C adapter registered
imx-i2c imx-i2c.2: <i2c_imx_probe>
imx-i2c imx-i2c.2: <i2c_imx_probe> bitrate:100000
i2c i2c-2: claimed irq 70
i2c i2c-2: device resources from 0x21a8000 to 0x21a8fff
i2c i2c-2: allocated 4096 bytes at 0x21a8000
i2c i2c-2: adapter name: "imx-i2c"
i2c i2c-2: IMX I2C adapter registered
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
i2c-core: driver [max17135] using legacy suspend method
i2c-core: driver [max17135] using legacy resume method
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 32
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = c0880000 suspend_iram_base=c091c000
PM driver module loaded
IMX PCIe port: link up.
pci 0000:00:00.0: [16c3:abcd] type 1 class 0x000604
pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff 64bit pref]
pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]
pci 0000:00:00.0: supports D1
pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
pci 0000:00:00.0: PME# disabled
PCI: bus0: Fast back to back transfers disabled
pci 0000:01:00.0: [14f1:8580] type 0 class 0x000400
pci 0000:01:00.0: reg 10: [mem 0x00000000-0x001fffff 64bit]
pci 0000:01:00.0: supports D1 D2
pci 0000:01:00.0: PME# supported from D0 D1 D2 D3hot
pci 0000:01:00.0: PME# disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:00:00.0: BAR 8: assigned [mem 0x01200000-0x013fffff]
pci 0000:00:00.0: BAR 0: assigned [mem 0x01100000-0x011fffff 64bit pref]
pci 0000:00:00.0: BAR 0: set to [mem 0x01100000-0x011fffff 64bit pref] (PCI address [0x1100000-0x11fffff])
pci 0000:00:00.0: BAR 6: assigned [mem 0x01400000-0x0140ffff pref]
pci 0000:01:00.0: BAR 0: assigned [mem 0x01200000-0x013fffff 64bit]
pci 0000:01:00.0: BAR 0: set to [mem 0x01200000-0x013fffff 64bit] (PCI address [0x1200000-0x13fffff])
pci 0000:00:00.0: PCI bridge to [bus 01-01]
pci 0000:00:00.0: bridge window [io disabled]
pci 0000:00:00.0: bridge window [mem 0x01200000-0x013fffff]
pci 0000:00:00.0: bridge window [mem pref disabled]
IMX usb wakeup probe
the wakeup pdata is 0xbfcf6040
add wake up source irq 75
IMX usb wakeup probe
the wakeup pdata is 0xbfcf6c80
cpu regulator init ldo=1
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
msgmni has been set to 1750
alg: No test for stdrng (krng)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
valid mode RGB666
_regulator_get: get() with no identifier
mxc_ldb mxc_ldb: ldb_clk to di clk: ldb_di0_clk -> ipu1_di0_clk
mxc_ldb mxc_ldb: Single mode channel 0 route to IPU0-DI0
Inside ldb_disp_setup pixel_clk:64998000 rounded_pixel_clk:64653061
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
mxc_sdc_fb mxc_sdc_fb.0: ### fb_blank line:1039
mxc_sdc_fb mxc_sdc_fb.0: blank = 0
Inside ldb_disp_setup pixel_clk:64998000 rounded_pixel_clk:64653061
Console: switching to colour frame buffer device 170x48
mxc_sdc_fb mxc_sdc_fb.0: mxcfb_pan_display line:1399
### Called fb_pan_display err:-22
mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb
valid mode RGB666
mxc_ldb mxc_ldb: for second ldb displdb mode should in separate mode
mxc_sdc_fb mxc_sdc_fb.1: NO mxc display driver found!
mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd
mxc_sdc_fb mxc_sdc_fb.2: ipu0-di0 already in use
mxc_sdc_fb: probe of mxc_sdc_fb.2 failed with error -16
mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb
valid mode RGB666
mxc_ldb mxc_ldb: for second ldb displdb mode should in separate mode
mxc_sdc_fb mxc_sdc_fb.3: NO mxc display driver found!
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
console [ttymxc2] enabled, bootconsole disabled
loop: module loaded
Can't recover from RESET HBA!
No sata disk.
m25p80 spi0.0: found m25p32, expected sst25vf016b
m25p80 spi0.0: m25p32 (4096 Kbytes)
Creating 2 MTD partitions on "m25p80":
0x000000000000-0x000000100000 : "bootloader"
0x000000100000-0x000000400000 : "kernel"
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
wait otg vbus change timeout!
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
lirc_dev: IR Remote Control driver registered, major 252
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR LIRC bridge handler initialized
Linux video capture interface: v2.00
In MVC: init_camera_struct
In MVC: init_camera_struct
###### Inside prp_enc_init line:584
###### Inside csi_enc_init line:423
In adv7180_init
DBG sensor data is at 80b9d6b8
In adv7180_probe
Inside mx6q_csi0_io_init_adv7441 line:564
Inside mx6q_csi0_io_init_adv7441 line:577 init high
Inside mx6q_csi0_io_init_adv7441 line:581 set low
Inside mx6q_csi0_io_init_adv7441 line:588 set high
Inside mx6q_csi0_cam_powerdown_adv7441 line:559
adv7441a 1-0021: adv7180_probe:adv7180 probe i2c address is 0x21
adv7441a 1-0021: adv7180_probe:Analog Device adv7 00 detected!
adv7441a 1-0021: In adv7180:adv7180_hard_reset
###### adv7180_write_reg reg:0x0 val:0xe
###### adv7180_write_reg reg:0x3 val:0x0
###### adv7180_write_reg reg:0x4 val:0x47
###### adv7180_write_reg reg:0x5 val:0x0
###### adv7180_write_reg reg:0x3c val:0xad
###### adv7180_write_reg reg:0x17 val:0x41
###### adv7180_write_reg reg:0x67 val:0x2
###### adv7180_write_reg reg:0x68 val:0xf0
###### adv7180_write_reg reg:0x1d val:0x40
###### adv7180_write_reg reg:0x31 val:0x1a
###### adv7180_write_reg reg:0x32 val:0x81
###### adv7180_write_reg reg:0x33 val:0x84
###### adv7180_write_reg reg:0x34 val:0x0
###### adv7180_write_reg reg:0x35 val:0x0
###### adv7180_write_reg reg:0x36 val:0x7d
###### adv7180_write_reg reg:0x37 val:0xa1
###### adv7180_write_reg reg:0x3a val:0x7
###### adv7180_write_reg reg:0x3c val:0xa8
###### adv7180_write_reg reg:0x47 val:0xa
###### adv7180_write_reg reg:0xba val:0xa0
###### adv7180_write_reg reg:0xf3 val:0x7
###### adv7180_write_reg reg:0x69 val:0x0
###### adv7180_write_reg reg:0xe8 val:0x41
###### adv7180_write_reg reg:0xe9 val:0x84
###### adv7180_write_reg reg:0xea val:0x6
type is 2 (expect 2)
num ioctls is 11
adv7441a 1-0021: adv7180:ioctl_s_power
adv7441a 1-0021: adv7180:ioctl_g_fmt_cap
Returning size of 720x625
End of mxc_v4l2_master_attach: device_type 1
End of mxc_v4l2_master_attach: v2f pix widthxheight 288 x 352
End of mxc_v4l2_master_attach: crop_bounds widthxheight 720 x 625
End of mxc_v4l2_master_attach: crop_defrect widthxheight 720 x 625
End of mxc_v4l2_master_attach: crop_current widthxheight 720 x 625
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
gspca: v2.13.0 registered
cx25858 driver version 2.0.111 loaded
cx25858 driver register unsuccess
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCIATH3K protocol initialized
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci sdhci-esdhc-imx.3: support_8bit:1
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA
sdhci sdhci-esdhc-imx.1: support_8bit:1
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA
sdhci sdhci-esdhc-imx.2: support_8bit:1
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
Thermal calibration data is 0x5784c37d
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
Registered led device: chg_now_led
ehci_fsl_bus_suspend begins, DR
ehci_fsl_bus_suspend ends, DR
ehci_fsl_bus_suspend begins, Host 1
ehci_fsl_bus_suspend ends, Host 1
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
Cirrus Logic CS42888 ALSA SoC Codec Driver
i2c-core: driver [cs42888] using legacy suspend method
i2c-core: driver [cs42888] using legacy resume method
imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12
imx_3stack asoc driver
ALSA device list:
No soundcards found.
NET: Registered protocol family 26
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 SEM08G 7.39 GiB
mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB
mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB
mmcblk0: p1
can: broadcast manager protocol (rev 20090105 t)
mmcblk0boot1: unknown partition table
Bluetooth: RFCOMM TTY layer initialized
mmcblk0boot0: unknown partition table
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
lib80211: common routines for IEEE802.11 drivers
lib80211_crypt: registered algorithm 'NULL'
lib80211_crypt: registered algorithm 'WEP'
lib80211_crypt: registered algorithm 'CCMP'
lib80211_crypt: registered algorithm 'TKIP'
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 02:29:39 UTC (8979)
EXT2-fs (mmcblk0p1): warning: mounting unchecked fs, running e2fsck is recommended
VFS: Mounted root (ext2 filesystem) on device 179:1.
Freeing init memory: 212K
udevd (1458): /proc/1458/oom_adj is deprecated, please use /proc/1458/oom_score_adj instead.
mmc2: new high speed SDHC card at address 1234
mmcblk1: mmc2:1234 SA08G 7.28 GiB
mmcblk1: p1
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 234449
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 234449
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 234449
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 363702
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 363702
EXT2-fs (mmcblk0p1): error: ext2_lookup: deleted inode referenced: 363702
### fbcon_blank line:2308
### fbcon_blank line:2330
mxc_sdc_fb mxc_sdc_fb.0: ### fb_blank line:1039
mxc_sdc_fb mxc_sdc_fb.0: blank = 1
root@freescale ~$
root@freescale ~$ lspci -v
00:00.0 Class 0604: 16c3:abcd
01:00.0 Class 0400: 14f1:8580
root@freescale ~$
but my pci device driver cx25858 cannot register,
Solved! Go to Solution.
Hi
Thanks for moving here.
I checked the codes, 1.1.0 release doesn't support MSI, only the legacy INTx mode is supported.
Standard PCIe EP should work well in Legacy INTx mode when MSI is not supported, refer to the PCI/PCIE SPEC.
Regarding to your log, the memory space required by PCIe EP device had been allocated by PCIe RC already.
The PCIe link is up, PCI/PCIe bus enumeration had been completed.
In the other words, the clocks, power, and memory map had been ready. and the PCIe EP is ready to use.
I don't know the exact reason why your driver can't register.
The PCIe link is up, PCI/PCIe bus enumeration had been completed.
Can you trace into the codes and figure out the root cause?
Best Regards
Richard.
static struct pci_device_id cx25858_pci_tbl[] = {
{
/* CX25858 Atlas Plus */
.vendor = 0x14f1,
.device = 0x8580,
.subvendor = 0x14f1,
.subdevice = 0x0950,
....................................................................................................................................................
if (!pci_register_driver(&cx25858_pci_driver)) {
pci_unregister_driver(&cx25858_pci_driver);
printk(KERN_INFO "cx25858 driver unsuccess\n");
return -ENODEV;
}
printk(KERN_INFO "cx25858 driver success\n");
return 0;
}
Hi
Thanks for moving here.
I checked the codes, 1.1.0 release doesn't support MSI, only the legacy INTx mode is supported.
Standard PCIe EP should work well in Legacy INTx mode when MSI is not supported, refer to the PCI/PCIE SPEC.
Regarding to your log, the memory space required by PCIe EP device had been allocated by PCIe RC already.
The PCIe link is up, PCI/PCIe bus enumeration had been completed.
In the other words, the clocks, power, and memory map had been ready. and the PCIe EP is ready to use.
I don't know the exact reason why your driver can't register.
The PCIe link is up, PCI/PCIe bus enumeration had been completed.
Can you trace into the codes and figure out the root cause?
Best Regards
Richard.
BTW, The following devices had been tested on 1.1.0 releases.
* Intel e1000e network card
* Intel iwl4965, 5100, 620, and 630 wifi cards
* xHCI PCIe2USB3.0 card.
Best Regards
Richard.
Thanks。I get it,but why remove always after probe :
***********************************
cx25858 init dev
***********************************
cx25858[0]/0: cx25858_set_tvnorm(norm = 0x00001000) name: [NTSC-M]
cx25858_ioctl_register(), dev = cx25858-ioctl0, board = 0
cx25858(0): cx25858 setup done!
install board = 0
cx25858[0]/0: found at 0000:01:00.0, rev: 1, irq: 155, latency: 0, mmio: 0x1200000
***********************************
Remove cx25858 device 0
***********************************
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_set_tvnorm(norm = 0x00001000) name: [NTSC-M]
cx25858_ioctl_register(), dev = cx25858-ioctl0, board = 0
cx25858(0): cx25858 setup done!
install board = 0
cx25858[0]/0: found at 0000:01:00.0, rev: 1, irq: 155, latency: 0, mmio: 0x1200000
‘’‘’‘’‘’‘’‘
***********************************
Remove cx25858 device 0
***********************************
Free pci_dev->irq
/dev/video4 is released!
/dev/video5 is released!
/dev/video6 is released!
/dev/video7 is released!
/dev/video8 is released!
/dev/video9 is released!
/dev/video10 is released!
/dev/video11 is released!
/dev/video12 is released!
unregister cx25858-ioctl0
cx25858-ioctl unloaded properly.
cx25858(0): Releasing lmmio.
why remove ?because __devexit_p ?
Thanks
HI
root@freescale /sys/bus$ ls
ac97 hid mmc scsi spi
amba i2c pci sdio usb
event_source mdio_bus platform serio
root@freescale /sys/bus$ cd pci/
root@freescale /sys/bus/pci$ ll
drwxr-xr-x 2 root root 0 Jan 1 00:00 devices
drwxr-xr-x 3 root root 0 Jan 1 00:00 drivers
-rw-r--r-- 1 root root 4096 Jan 1 00:06 drivers_autoprobe
--w------- 1 root root 4096 Jan 1 00:06 drivers_probe
--w--w---- 1 root root 4096 Jan 1 00:06 rescan
-rw-r--r-- 1 root root 4096 Jan 1 00:06 resource_alignment
drwxr-xr-x 2 root root 0 Jan 1 00:06 slots
--w------- 1 root root 4096 Jan 1 00:00 uevent
root@freescale /sys/bus/pci$
root@freescale /sys/bus/pci$
root@freescale /sys/bus/pci$ cd devices/
root@freescale /sys/bus/pci/devices$ ls
0000:00:00.0 0000:01:00.0
root@freescale /sys/bus/pci/devices$ cd ..
root@freescale /sys/bus/pci$ cd drivers
root@freescale /sys/bus/pci/drivers$ ll
drwxr-xr-x 2 root root 0 Jan 1 00:00 ehci_hcd
root@freescale /sys/bus/pci/drivers$ cd ehci_hcd/
root@freescale /sys/bus/pci/drivers/ehci_hcd$ ls
bind module new_id remove_id uevent unbind
root@freescale /sys/bus/pci/drivers/ehci_hcd$
root@freescale /sys/bus/pci/drivers/ehci_hcd$ lspci
00:00.0 Class 0604: 16c3:abcd
01:00.0 Class 0400: 14f1:8580
root@freescale /sys/bus/pci/drivers/ehci_hcd$
Sorry !
the log is:
***********************************
cx25858 init dev
***********************************‘
‘’‘’‘’‘’‘’‘
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_vdev_init()
cx25858[0]/0: cx25858_set_tvnorm(norm = 0x00001000) name: [NTSC-M]
cx25858_ioctl_register(), dev = cx25858-ioctl0, board = 0
cx25858(0): cx25858 setup done!
install board = 0
cx25858[0]/0: found at 0000:01:00.0, rev: 1, irq: 155, latency: 0, mmio: 0x1200000
***********************************
Remove cx25858 device 0
***********************************
Free pci_dev->irq
/dev/video4 is released!
/dev/video5 is released!
/dev/video6 is released!
/dev/video7 is released!
/dev/video8 is released!
/dev/video9 is released!
/dev/video10 is released!
/dev/video11 is released!
/dev/video12 is released!
unregister cx25858-ioctl0
cx25858-ioctl unloaded properly.
cx25858(0): Releasing lmmio.