imx6q "formatting rootfs partition" problem using MFGTools v2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q "formatting rootfs partition" problem using MFGTools v2

2,681 次查看
baptistea
Contributor I

Hi guys,

I am trying to update the Linux version I had on a imx6-q SABRE-SD board. I didn't install the previous version and I never installed a Linux this way in my life, i.e. I am totally new with this. Anyway I followed a Guide to Flash a SD card with the right Linux version I wanted (L3.0.35-4.1.0) and I managed to launch MFG Tools the right way I think but it bugged at the step "Formatting rootfs partition".

I saw that it could be a lack of space when the partitioning have been done just before. I looked up this info and noticed that the partitioning was building on my SD card was only 80MB while the oneiric file containing the Linux was almost 800 MB. I edited the right file (mksdcard.sh.tar) to choose 800MB.

Here is the XML part showing the partitioning / formatting ... :

<CMD state="Updater" type="push" body="send" file="mksdcard.sh.tar">Sending partition shell</CMD>
<CMD state="Updater" type="push" body="$ tar xf $FILE "> Partitioning...</CMD>
<CMD state="Updater" type="push" body="$ sh mksdcard.sh /dev/mmcblk1"> Partitioning...</CMD>

    <CMD state="Updater" type="push" body="$ mkfs.ext3 -j /dev/mmcblk1p1">Formatting rootfs partition</CMD>
    <CMD state="Updater" type="push" body="$ mkdir -p /mnt/mmcblk1p1"/>
    <CMD state="Updater" type="push" body="$ mount -t ext3 /dev/mmcblk1p1 /mnt/mmcblk1p1"/>
    <CMD state="Updater" type="push" body="pipe tar --numeric-owner -zxv -C /mnt/mmcblk1p1" file="files/oneiric.tgz">Sending and writting rootfs</CMD>
    <CMD state="Updater" type="push" body="frf">Finishing rootfs write</CMD>
    <CMD state="Updater" type="push" body="$ umount /mnt/mmcblk1p1">Unmounting rootfs partition</CMD>
    <CMD state="Updater" type="push" body="$ echo Update Complete!">Done</CMD>

I hope some of you have info about that.

Baptiste

标记 (1)
0 项奖励
回复
3 回复数

1,679 次查看
LeonardoSandova
Specialist I

The MFG Tool undestand XML commands, and if you want to change something on the mksdcard script, then you have to 'untar & change & tar'. Also, make sure the SD is at least 4G.

Leo

1,679 次查看
baptistea
Contributor I

I found a way to correct my problem : dont try to flash a SabreSD while I only have a SabreLite >< The partitioning/formatting was not my problem here !!

0 项奖励
回复

1,679 次查看
LeonardoSandova
Specialist I

Got it. That is a typical problem: choosing the wrong profile. In the other hand, try flashing the SD unde a Linux OS, you will understand what the script is actually doing :smileyhappy:

Leo

0 项奖励
回复