imx6q pcie bar空间的扩展

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q pcie bar空间的扩展

Jump to solution
1,793 Views
bianlei
Contributor I

你好,我现在使用imx6q芯片来更新升级一个项目,其中需要使用imx6q来替换原本的x86,在原本项目上,作为ep端的是一个DSP设备,其中该dsp设备的bar空间为 2*256M(即两个大的空间,每个256M),现在使用imx6q来替换后,在启动log信息中,看到信息指示不能分配这么大的空间。我想确认一下,是否imx6q上的pcie bar空间只有14M,不能通过别的方式来进行增加(例如通过修改特定寄存器中内容,让原本分配到ddr中的一部分地址空间给pcie来使用,因为imx6上ddr空间有3.8G,我们现在只是用了2G,剩下的地址空间是否能给pcie使用),如果有别的方法可以增加pcie 的bar空间,也请告诉我,期待你的回复。

Labels (1)
0 Kudos
1 Solution
2 Replies
1,150 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
1,148 Views
chqing
Contributor I

你好,PCIE  总出现下面连接的需求,

https://community.nxp.com/thread/308436#

照着这个patch 更改后,并未发现这个BAR0 地址有所变化?麻烦给下技术支持。

0 Kudos