imx6q mxc_sdc_fb timeout when waiting for flip irq

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6q mxc_sdc_fb timeout when waiting for flip irq

跳至解决方案
31,946 次查看
moseeneview
Contributor II

sometimes, my imx6q board gets timeout when waiting for flip irq    with rate 10~20%.

mxc_ipuv3_fb.c:

          it seems there's not irq to do complete. and then it wait_for_completion_timeout.

hwcomposer/hwc_vsync.cpp

          FBIO_WAITFORVSYNC error: time expire

i try as below, the issue also come out sometime. could u tell me why or some advice. thx.

1) Wait longer:    wait_for_completion_timeout(&mxc_fbi->flip_complete, 4*HZ);

2)  ldb_data = {

        .ipu_id = 1,          # or use ipu 0

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SIN0,

  }

      or

ldb_data = {

        .ipu_id = 1,

        .disp_id = 0,

        .ext_ref = 1,

        .mode = LDB_SEP0,

        .sec_ipu_id = 1,

        .sec_disp_id =1,

}

3) fb_data = {

    { /*fb0*/

    .disp_dev = "ldb",

    .interface_pix_fmt = IPU_PIX_FMT_RGB666,

    .mode_str = "LDB-XGA",

    .default_bpp = 16,

    .int_clk = false,

    .late_init = true,             # or false

    },

}

4)

ipu_data[] = {

    {

    .rev = 4,

    .csi_clk[0] = "clko_clk",

    .bypass_reset = false,

    }, {

    .rev = 4,

    .csi_clk[0] = "clko_clk",

    .bypass_reset = false,

    },

};

1 解答
18,687 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
29 回复数
18,688 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
10,941 次查看
Rayn_Jang
Contributor I

I am getting boot errors related to Errata ERR009624.

Booting error is output as below and LCD is not output.

The problem occurs in CPU Silicon Revision V1.1, and it works well in Silicon Revision V1.0.

Can you tell me if there is a patch code that works with CPU Silicon Revision V1.1 and V1.0?

 

Error Log Messages =====================================================

[ 12.039727] init: Starting service 'keystore'...
[ 12.040849] init: cannot find '/system/bin/rild', disabling 'ril-daemon'
[ 12.041015] init: Starting service 'zygote'...
[ 12.041703] init: Starting service 'gatekeeperd'...
[ 12.051618] init: Starting service 'perfprofd'...
[ 12.052422] init: Starting service 'magd'...
[ 12.258147] android_work: sent uevent USB_STATE=CONNECTED
[ 12.285786] configfs-gadget gadget: high-speed config #1: b
[ 12.291904] android_work: sent uevent USB_STATE=CONFIGURED
[ 12.706534] init: Service 'magd' (pid 270) exited with status 255
[ 13.264230] drivers/video/fbdev/mxc/ldb.c : ldb_disable
[ 13.264282] imx-ipuv3 2800000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000
[ 14.276377] imx-prg 21cd000.prg: wait for buffer ready timeout
[ 14.276894] drivers/video/fbdev/mxc/ldb.c : ldb_enable
[ 15.285237] imx-pre 21cb000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[ 15.407529] init: Starting service 'bootanim'...
[ 16.405411] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 17.405335] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 18.405280] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 18.480366] random: nonblocking pool is initialized
[ 19.405291] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 20.405287] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 21.386198] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
[ 21.405333] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 22.405310] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[ 23.405270] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0

=========================================================================

Best regards,

James.W

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

at the same time, i get ipu1_task "D" status,  and then the screen can't display anything.   log attached.

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 1 address=0x32180000

mxc_sdc_fb mxc_sdc_fb.0: Update complete

warning: `zygote' uses 32-bit capabilities (legacy support in use)

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

request_suspend_state: wakeup (3->0) at 19259779337 (1970-01-01 00:00:12.7501263                                             35 UTC)

cpufreq_interactive_input_connect: connect to ft5x0x_ts

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 2 address=0x32300000

mxc_sdc_fb mxc_sdc_fb.0: Update complete

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32000000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32000000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32180000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32180000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32300000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32300000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:06, irq=-1)

ADDRCONF(NETDEV_UP): eth0: link is not ready

acc_open

acc_release

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

ehci_fsl_bus_resume begins, Host 1

ehci_fsl_bus_resume ends, Host 1

ehci_fsl_bus_resume begins, DR

ehci_fsl_bus_suspend begins, Host 1

ehci_fsl_bus_suspend ends, Host 1

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32000000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32000000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32180000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32180000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32300000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32300000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32000000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32000000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32180000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32180000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

init: sys_prop: permission denied uid:1003  name:service.bootanim.exit

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32300000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32300000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32000000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32000000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32180000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32180000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: Y wrap disabled

mxc_sdc_fb mxc_sdc_fb.0: timeout when waiting for flip irq

mxc_sdc_fb mxc_sdc_fb.0: Updating SDC DISP4 BG buf 0 address=0x32300000

mxc_sdc_fb mxc_sdc_fb.0: Error updating SDC buf 0 to address=0x32300000, current                                              buf 2, buf0 ready 1, buf1 ready 1, buf2 ready 1

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

mxc_sdc_fb mxc_sdc_fb.0: MXCFB_WAIT_FOR_VSYNC: timeout 0

0 项奖励
回复
14,494 次查看
ji_yun
Contributor II

Hi Mosee,

I met this same issue,you have solve this issue later? Have any advices?

 

Thanks,

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II
0 项奖励
回复
14,543 次查看
jamesbone
NXP TechSupport
NXP TechSupport

We are analyzing your inquiry can you please let us know if,  waht board are you using? and what Linux BSP ?

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

hi, jamesbone. thx for your reply.   we're using   imx6q custom board based on sabresd with jb4.3 1.1.0 bsp.

0 项奖励
回复
14,543 次查看
jamesbone
NXP TechSupport
NXP TechSupport

But how do you run into this case? Is the framebuffer driver in blanking state at that time?

0 项奖励
回复
14,543 次查看
karina_valencia
NXP Apps Support
NXP Apps Support
Re: imx6q mxc_sdc_fb timeout when waiting for flip irq

Qiang LiEmployee

From the log we can only know the IPU display is not working correctly. But how do the customer run into this case? Is the framebuffer driver in blanking state at that time?

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

In a mater of fact, i haven't found out the real reason. But when i power

off/on my device time and time again, it'll run into this case randomly.

Besides, what do u mean blanking state?

On Tue, Apr 22, 2014 at 10:43 PM, Karina Valencia Aguilar <

0 项奖励
回复
14,543 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

If the IPU display IDMAC is not enabled (framebuffer in blanking state), the PAN display will get such timeout information.

And if the IDMAC is in wrong state, it can also make PAN display timeout.

Maybe you can add more debug messages in ipu_common.c to check the IDMAC, such as ipu_disable_channel(), ipu_enable_channel(), ipu_init_channel(), ipu_uninit_channel().

14,543 次查看
moseeneview
Contributor II

hi Qiang Li,  I didn't get IDMAC error.  and i get this issue rondomly, not always.

0 项奖励
回复
14,543 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

"Power off/on the device" is it suspend/resume test or power off/on reboot test? If it is the whole system reboot, can you attach the whole kernel boot log?

What's your display device? LCD, LVDS, HDMI? Single display or multi-display? Did you change any IPU related code in your BSP? In whcih case will you do the suspend/resume? Just idle on home screen?

14,543 次查看
JithCR
Contributor III

I am also facing the same kind display issue with "mxc_sdc_fb timeout when waiting for flip irq" message.I am doing power ON and OFF for getting the issue.Our display device is LVDS,single display.We did  not make any change in IPU related code.

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

hey, Jith CR. have u find sth about the issue?

On Mon, May 26, 2014 at 6:21 PM, Jith CR <admin@community.freescale.com>

0 项奖励
回复
14,543 次查看
JithCR
Contributor III

Hi Mosee,

I am trying to find out sth more about the issue.

Have you solved the issue?

Please share, if you have more information about the issue.

Regards,

Jith

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

not yet.

i try to improve LCD timing(ldb) which is matter with ipu.

and then it seems to cut down the rate.

but i haven't solved this issue yet.

On Sat, May 31, 2014 at 2:52 PM, Jith CR <admin@community.freescale.com>

0 项奖励
回复
14,543 次查看
pfsang
Contributor IV

hi, Mosee

i encounter  this same issue during system boot, do you have solved this issue later? Have any advices?

Thanks,

peter

0 项奖励
回复
14,543 次查看
moseeneview
Contributor II

hey, fang min. i haven't solved yet. but u can have a try to improve it as

below what i mentioned before.

On Thu, Jun 19, 2014 at 6:51 PM, fang min <admin@community.freescale.com>

0 项奖励
回复
14,494 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi Mosee Neview, I think you should make sure the IPU plat_data->bypass_reset should be false in ipu_common.c, function ipu_probe().

If bypass_reset is true, the IPU will not be fully initialized.

Kernel config "CONFIG_MX6_CLK_FOR_BOOTUI_TRANS=y" should be removed, and in kernel boot command line, "fb0base=0x27b00000" should be removed too.

On Freescale original BSP, the LVDS panel will be enabled in Uboot, then in kernel, some IPU re-initialization code will be skipped, but on your board, if you had used other dispay device, or you had used other IPU DI port, this setting will get the flip irq error.

This can be double checked in kernel boot up log, if there is two IPU probe information together, that means the two IPU had been initialized fully, if in early log, there is only one IPU probe log, and another IPU's log appears when Android logo displayed, that means that IPU had been bypassed reset:

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

0 项奖励
回复