imx6q how to change enet rgmii tx clock's phase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q how to change enet rgmii tx clock's phase

307件の閲覧回数
muryliang
Contributor I

I use  imx6q custom board's mac to connect a fpga board, which is used as the phy side, and use rgmii mode. I have configured fixed-link and set speed as 1000,  now   send and recv can work fine.  But when I keep sending packet from imx6q to fpga board, sometimes package will lose.    I think it may because the tx clock and txdata are too close, so I want to change tx clock phase by 90 degree,  how can I do that, where in the code modify? 

タグ(1)
0 件の賞賛
返信
0 返答(返信)