I use MCIMX6Q-SDB board to test hdmi interface, use hdmi-vga adapter to connect pc display, but display nothing.
image is linux 3.0.35,supplied by freescale.
1.uboot bootargs is :
console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=hdmi,1920x1080M@60 video=mxcfb1:off video=mxcfb2:off fbmem=28M
2.after system start, some parameters are :
cd /sys/devices/platform/mxc_hdmi
cat cable_state
plugin
cat edid
0(all is 0)
cat hdcp_enable
hdcp disable
cat rgb_out_enable
RGB out
cat fb_name
DISP3 BG
cd /sys/class/graphics/fb0/
cat modes
U:1280x720p-120
U:1280x720p-100
U:1920x1080p-30
U:1920x1080p-25
U:1920x1080p-24
U:1920x1080p-50
U:1440x576p-50
U:1440x576p-50
U:1440x288p-50
U:1440x288p-50
U:1280x720p-50
U:720x576p-50
U:720x576p-50
U:1920x1080p-60
U:1440x480p-60
U:1440x480p-60
U:1440x240p-60
U:1440x240p-60
U:1280x720p-60
U:720x480p-60
U:720x480p-60
U:640x480p-60
V:1280x1024p-60
V:1024x768p-60
V:640x480p-60
cat mode
U:1920x1080p-60
cat fsl_disp_dev_property
hdmi
3.plug in hdmi ,kernel log is
mxc_hdmi mxc_hdmi: Read EDID again
mxc_hdmi mxc_hdmi: No modes read from edid
mxc_hdmi mxc_hdmi: create default modelist
I want to know why imx6q hdmi can't display.
thanks Miles。
I will buy one to test.
One more question:
I use hmdi cable to connect TV, android os can display normal.But linux os (rootfs.tar.bz2 or ubuntu_oneiric_4.1.0.tgz) can't display.
I compare the uboot args, cable_state / modes / mode / edid parameters,those are the same.
After system boot , i find Xorg start failed. I download oneiric.tar again from freescale 。But , Xorg start failed again.
The log is :
root@linaro-ubuntu-desktop:~# export DISPLAY=:0.0
root@linaro-ubuntu-desktop:~# Xorg
_XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6
_XSERVTransOpen: transport open failed for inet6/linaro-ubuntu-desktop:0
_XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6
X.Org X Server 1.10.4
Release Date: 2011-08-19
X Protocol Version 11, Revision 0
Build Operating System: Linux 2.6.35-24-omap armv7l Ubuntu
Current Operating System: Linux linaro-ubuntu-desktop 3.0.35-2666-gbdde708-gf3d259a-dirty #38 SMP PREEMPT Wed Sep 9 22:11:17 CST 2015 armv7l
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p1 rootwait vmalloc=400M video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 video=mxcfb1:off video=mxcfb2:off fbmem=28M
Build Date: 19 October 2011 06:22:31AM
xorg-server 2:1.10.4-1ubuntu4.2 (For technical support please see http://www.ubuntu.com/support)
Current version of pixman: 0.22.2
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan 1 00:10:16 1970
(==) Using config file: "/etc/X11/xorg.conf"
Backtrace:
Segmentation fault at address 0xc
Caught signal 11 (Segmentation
==== system start log is :
modprobe: FATAL: Could not load /lib/modules/3.0.35-2666-gbdde708-gf3d259a-dirty/modules.dep: No such file or directory
error: unexpectedly disconnected from boot status daemon
* Starting Advanced Power Management daemon... [ OK ]
Last login: Thu Jan 1 00:02:09 UTC 1970 on tty1
speech-dispatcher disabled; edit /etc/default/speech-dispatcher
Checking for running unattended-upgrades:
/usr/lib/update-notifier/update-motd-updates-available: 52: cannot create /var/lib/update-notifier/updates-available: Directory nonexistent
run-parts: /etc/update-motd.d/90-updates-available exited with return code 2
/usr/lib/update-manager/release-upgrade-motd: 40: cannot create /var/lib/update-notifier/release-upgrade-available: Directory nonexistent
cat: /var/lib/update-notifier/fsck-at-reboot: No such file or directory
run-parts: /etc/update-motd.d/98-fsck-at-reboot exited with return code 1
root@linaro-ubuntu-desktop:~# * Starting bluetooth [ OK ]
* PulseAudio configured for per-user sessions
saned disabled; edit /etc/default/saned
1 Jan 00:02:11 ntpdate[5251]: no servers can be used, exiting
Ps:uImage is compiled by myself and emmc boot.