imx6q governor: performance and powersave - USB support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q governor: performance and powersave - USB support

886件の閲覧回数
aleksmish
Contributor I

We have a board, similar to the SabreLite.

If the kernel configuration with powersave governor and USB support (ECHI 2.0 hub) then board is loaded, but does not work at temperatures below 5 degrees Celsius.

If the kernel configuration with performance governor and USB support (ECHI 2.0 hub) then board is not loaded. loading stops after initialization DVFS and before or during the initialization of USB and then nothing happens with the board.

If the kernel configuration with performance governor and without USB support (ECHI 2.0 hub) then board is loaded and stably operates at a temperature below -30 degrees Celsius, but does not work USB bus. we need a USB bus.

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

767件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please check Your design, using recommendations of Design Checklist in Chapter 2 (Design
Checklist), Chapter 3 (i.MX 6 Series Layout Recommendations) and Chapter 8 (Avoiding Board
Bring-up Problems) of "Hardware Development Guide for i.MX 6Quad,6Dual, 6DualLite, 6Solo
Families". Please pay attention on USB considerations.

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

  Also, please try to test memory (under low temperature), using the Stress test.

“i.MX6 DDR Stress Test Tool V1.0.3”

https://community.freescale.com/docs/DOC-96412

DDR3 Porting Guide also may be useful for DDR Test Tool operations.

https://community.freescale.com/docs/DOC-101708


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

767件の閲覧回数
aleksmish
Contributor I

Yuri Muhin написал(а):

  Please check Your design, using recommendations of Design Checklist in Chapter 2 (Design
Checklist), Chapter 3 (i.MX 6 Series Layout Recommendations) and Chapter 8 (Avoiding Board
Bring-up Problems) of "Hardware Development Guide for i.MX 6Quad,6Dual, 6DualLite, 6Solo
Families". Please pay attention on USB considerations.

These recommendations are made, everything matches.

Test memory (under low temperature) is good. DDR3 is calibrated.

0 件の賞賛
返信