imx6q eim problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q eim problem

272 次查看
xjy198903
Contributor III

 

The EIM module of imx6q uses a 16-bit address line (AD0~AD15),16-bit data line (DA16~DA31), asynchronous mode, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line, the module is connected to FPGA, no matter it is read or write, the information on the data line is valid, but there is always no valid data on the address line.

 
标记 (1)
0 项奖励
回复
0 回复数