imx6q ddr test tool default uart baud rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q ddr test tool default uart baud rate

1,365 Views
建华董
Contributor I

Hi,all!

   I got a custom board based on MCIMX6Q6AVT10AE,now I attempt to test the ddr performance with 'ddr_stress_tester_jtag_v2.90'(for some reasons USB OTG did not work) , the cpu core starts to work after downloading the elf file into Ocram ,but the serail port txd Baud rate is 5760(not 115200), I can receive the data correctly with my serial port assistant tools,but CPU responses nothing to my command.I check  the signal with my oscilloscope and rxd data is all ok.How is this happening?Does the ddr_stress_tester_jtag_v2.90 tool set default Baud rate to 115200 ,or not?

Labels (1)
0 Kudos
Reply
1 Reply

1,263 Views
jimmychan
NXP TechSupport
NXP TechSupport

yes, the default baud rate is 115200

0 Kudos
Reply