============================================
DDR Stress Test (2.6.0)
Build: Aug 1 2017, 17:33:25
NXP Semiconductors.
============================================
Chip ID
CHIP ID = i.MX6 Dual/Quad (0x63)
Internal Revision = TO1.5
============================================
============================================
Boot Configuration
SRC_SBMR1(0x020d8004) = 0x00005860
SRC_SBMR2(0x020d801c) = 0x31000001
============================================
ARM Clock set to 800MHz
============================================
DDR configuration
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 15, col size: 10
Chip select CSD0 is used
Density per chip select: 2048MB
============================================
Current Temperature: 51
============================================
DDR Freq: 528 MHz
ddr_mr1=0x00000000
Start write leveling calibration...
running Write level HW calibration
Write leveling calibration completed, update the following registers in your initialization script
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x001F0019
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x001F0023
MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x0018001F
MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x0006001F
Write DQS delay result:
Write DQS0 delay: 25/256 CK
Write DQS1 delay: 31/256 CK
Write DQS2 delay: 35/256 CK
Write DQS3 delay: 31/256 CK
Write DQS4 delay: 31/256 CK
Write DQS5 delay: 24/256 CK
Write DQS6 delay: 31/256 CK
Write DQS7 delay: 6/256 CK
Starting DQS gating calibration
. HC_DEL=0x00000000 result[00]=0x11111111
. HC_DEL=0x00000001 result[01]=0x01100111
. HC_DEL=0x00000002 result[02]=0x00100001
. HC_DEL=0x00000003 result[03]=0x00000000
. HC_DEL=0x00000004 result[04]=0x01000000
. HC_DEL=0x00000005 result[05]=0x11111111
. HC_DEL=0x00000006 result[06]=0x11111111
. HC_DEL=0x00000007 result[07]=0x11111111
. HC_DEL=0x00000008 result[08]=0x11111111
. HC_DEL=0x00000009 result[09]=0x11111111
. HC_DEL=0x0000000A result[0A]=0x11111111
. HC_DEL=0x0000000B result[0B]=0x11111111
. HC_DEL=0x0000000C result[0C]=0x11111111
. HC_DEL=0x0000000D result[0D]=0x11111111
DQS HC delay value low1 = 0x01020203, high1=0x04040404
DQS HC delay value low2 = 0x01020301, high2=0x04030404
loop ABS offset to get HW_DG_LOW
. ABS_OFFSET=0x00000000 result[00]=0x01000111
. ABS_OFFSET=0x00000004 result[01]=0x01000110
. ABS_OFFSET=0x00000008 result[02]=0x01000111
. ABS_OFFSET=0x0000000C result[03]=0x11011110
. ABS_OFFSET=0x00000010 result[04]=0x01000110
. ABS_OFFSET=0x00000014 result[05]=0x01000110
. ABS_OFFSET=0x00000018 result[06]=0x11011110
. ABS_OFFSET=0x0000001C result[07]=0x01000110
. ABS_OFFSET=0x00000020 result[08]=0x01000110
. ABS_OFFSET=0x00000024 result[09]=0x01000110
. ABS_OFFSET=0x00000028 result[0A]=0x11001110
. ABS_OFFSET=0x0000002C result[0B]=0x11000110
. ABS_OFFSET=0x00000030 result[0C]=0x00000110
. ABS_OFFSET=0x00000034 result[0D]=0x00000110
. ABS_OFFSET=0x00000038 result[0E]=0x10001110
. ABS_OFFSET=0x0000003C result[0F]=0x10011110
. ABS_OFFSET=0x00000040 result[10]=0x00000110
. ABS_OFFSET=0x00000044 result[11]=0x00000110
. ABS_OFFSET=0x00000048 result[12]=0x00010110
. ABS_OFFSET=0x0000004C result[13]=0x00000110
. ABS_OFFSET=0x00000050 result[14]=0x00000110
. ABS_OFFSET=0x00000054 result[15]=0x00000110
. ABS_OFFSET=0x00000058 result[16]=0x00000110
. ABS_OFFSET=0x0000005C result[17]=0x00010010
. ABS_OFFSET=0x00000060 result[18]=0x00000010
. ABS_OFFSET=0x00000064 result[19]=0x00000010
. ABS_OFFSET=0x00000068 result[1A]=0x00000010
. ABS_OFFSET=0x0000006C result[1B]=0x00000010
. ABS_OFFSET=0x00000070 result[1C]=0x00000000
. ABS_OFFSET=0x00000074 result[1D]=0x00000000
. ABS_OFFSET=0x00000078 result[1E]=0x00000000
. ABS_OFFSET=0x0000007C result[1F]=0x00000000
loop ABS offset to get HW_DG_HIGH
. ABS_OFFSET=0x00000000 result[00]=0x00000000
. ABS_OFFSET=0x00000004 result[01]=0x00000000
. ABS_OFFSET=0x00000008 result[02]=0x00000000
. ABS_OFFSET=0x0000000C result[03]=0x00000000
. ABS_OFFSET=0x00000010 result[04]=0x00000000
. ABS_OFFSET=0x00000014 result[05]=0x00000000
. ABS_OFFSET=0x00000018 result[06]=0x00000000
. ABS_OFFSET=0x0000001C result[07]=0x00000000
. ABS_OFFSET=0x00000020 result[08]=0x10000100
. ABS_OFFSET=0x00000024 result[09]=0x10000100
. ABS_OFFSET=0x00000028 result[0A]=0x10000100
. ABS_OFFSET=0x0000002C result[0B]=0x10101100
. ABS_OFFSET=0x00000030 result[0C]=0x10101100
. ABS_OFFSET=0x00000034 result[0D]=0x10101110
. ABS_OFFSET=0x00000038 result[0E]=0x10101110
. ABS_OFFSET=0x0000003C result[0F]=0x10111110
. ABS_OFFSET=0x00000040 result[10]=0x10111110
. ABS_OFFSET=0x00000044 result[11]=0x10111110
. ABS_OFFSET=0x00000048 result[12]=0x10111111
. ABS_OFFSET=0x0000004C result[13]=0x10111111
. ABS_OFFSET=0x00000050 result[14]=0x10111111
. ABS_OFFSET=0x00000054 result[15]=0x10111111
. ABS_OFFSET=0x00000058 result[16]=0x10111111
. ABS_OFFSET=0x0000005C result[17]=0x10111111
. ABS_OFFSET=0x00000060 result[18]=0x11111111
. ABS_OFFSET=0x00000064 result[19]=0x11111111
. ABS_OFFSET=0x00000068 result[1A]=0x11111111
. ABS_OFFSET=0x0000006C result[1B]=0x11111111
. ABS_OFFSET=0x00000070 result[1C]=0x11111111
. ABS_OFFSET=0x00000074 result[1D]=0x11111111
. ABS_OFFSET=0x00000078 result[1E]=0x11111111
. ABS_OFFSET=0x0000007C result[1F]=0x11111111
BYTE 0:
Start: HC=0x02 ABS=0x0C
End: HC=0x04 ABS=0x44
Mean: HC=0x03 ABS=0x28
End-0.5*tCK: HC=0x03 ABS=0x44
Final: HC=0x03 ABS=0x44
BYTE 1:
Start: HC=0x01 ABS=0x70
End: HC=0x04 ABS=0x30
Mean: HC=0x03 ABS=0x10
End-0.5*tCK: HC=0x03 ABS=0x30
Final: HC=0x03 ABS=0x30
BYTE 2:
Start: HC=0x01 ABS=0x5C
End: HC=0x04 ABS=0x1C
Mean: HC=0x02 ABS=0x7B
End-0.5*tCK: HC=0x03 ABS=0x1C
Final: HC=0x03 ABS=0x1C
BYTE 3:
Start: HC=0x00 ABS=0x40
End: HC=0x04 ABS=0x28
Mean: HC=0x02 ABS=0x34
End-0.5*tCK: HC=0x03 ABS=0x28
Final: HC=0x03 ABS=0x28
BYTE 4:
Start: HC=0x00 ABS=0x1C
End: HC=0x04 ABS=0x38
Mean: HC=0x02 ABS=0x2A
End-0.5*tCK: HC=0x03 ABS=0x38
Final: HC=0x03 ABS=0x38
BYTE 5:
Start: HC=0x02 ABS=0x00
End: HC=0x04 ABS=0x28
Mean: HC=0x03 ABS=0x14
End-0.5*tCK: HC=0x03 ABS=0x28
Final: HC=0x03 ABS=0x28
BYTE 6:
Start: HC=0x01 ABS=0x30
End: HC=0x03 ABS=0x5C
Mean: HC=0x02 ABS=0x46
End-0.5*tCK: HC=0x02 ABS=0x5C
Final: HC=0x02 ABS=0x5C
BYTE 7:
Start: HC=0x00 ABS=0x40
End: HC=0x04 ABS=0x1C
Mean: HC=0x02 ABS=0x2E
End-0.5*tCK: HC=0x03 ABS=0x1C
Final: HC=0x03 ABS=0x1C
DQS calibration MMDC0 MPDGCTRL0 = 0x03300344, MPDGCTRL1 = 0x0328031C
DQS calibration MMDC1 MPDGCTRL0 = 0x03280338, MPDGCTRL1 = 0x031C025C
Note: Array result[] holds the DRAM test result of each byte.
0: test pass. 1: test fail
4 bits respresent the result of 1 byte.
result 00000001:byte 0 fail.
result 00000011:byte 0, 1 fail.
Starting Read calibration...
ABS_OFFSET=0x00000000 result[00]=0x11111111
ABS_OFFSET=0x04040404 result[01]=0x11111111
ABS_OFFSET=0x08080808 result[02]=0x11111111
ABS_OFFSET=0x0C0C0C0C result[03]=0x11111111
ABS_OFFSET=0x10101010 result[04]=0x11111111
ABS_OFFSET=0x14141414 result[05]=0x01011111
ABS_OFFSET=0x18181818 result[06]=0x00011001
ABS_OFFSET=0x1C1C1C1C result[07]=0x00011000
ABS_OFFSET=0x20202020 result[08]=0x00010000
ABS_OFFSET=0x24242424 result[09]=0x00000000
ABS_OFFSET=0x28282828 result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000
ABS_OFFSET=0x30303030 result[0C]=0x00000000
ABS_OFFSET=0x34343434 result[0D]=0x00000000
ABS_OFFSET=0x38383838 result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000
ABS_OFFSET=0x40404040 result[10]=0x00000000
ABS_OFFSET=0x44444444 result[11]=0x00000000
ABS_OFFSET=0x48484848 result[12]=0x00000010
ABS_OFFSET=0x4C4C4C4C result[13]=0x00100010
ABS_OFFSET=0x50505050 result[14]=0x00100111
ABS_OFFSET=0x54545454 result[15]=0x01100111
ABS_OFFSET=0x58585858 result[16]=0x11100111
ABS_OFFSET=0x5C5C5C5C result[17]=0x11110111
ABS_OFFSET=0x60606060 result[18]=0x11111111
ABS_OFFSET=0x64646464 result[19]=0x11111111
ABS_OFFSET=0x68686868 result[1A]=0x11111111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x11111111
ABS_OFFSET=0x70707070 result[1C]=0x11111111
ABS_OFFSET=0x74747474 result[1D]=0x11111111
ABS_OFFSET=0x78787878 result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111
Byte 0: (0x1c - 0x4c), middle value:0x34
Byte 1: (0x18 - 0x44), middle value:0x2e
Byte 2: (0x18 - 0x4c), middle value:0x32
Byte 3: (0x20 - 0x5c), middle value:0x3e
Byte 4: (0x24 - 0x58), middle value:0x3e
Byte 5: (0x14 - 0x48), middle value:0x2e
Byte 6: (0x18 - 0x50), middle value:0x34
Byte 7: (0x14 - 0x54), middle value:0x34
MMDC0 MPRDDLCTL = 0x3E322E34, MMDC1 MPRDDLCTL = 0x34342E3E
Starting Write calibration...
ABS_OFFSET=0x00000000 result[00]=0x11111111
ABS_OFFSET=0x04040404 result[01]=0x11111111
ABS_OFFSET=0x08080808 result[02]=0x10110111
ABS_OFFSET=0x0C0C0C0C result[03]=0x10110110
ABS_OFFSET=0x10101010 result[04]=0x10100000
ABS_OFFSET=0x14141414 result[05]=0x10000000
ABS_OFFSET=0x18181818 result[06]=0x00000000
ABS_OFFSET=0x1C1C1C1C result[07]=0x00000000
ABS_OFFSET=0x20202020 result[08]=0x00000000
ABS_OFFSET=0x24242424 result[09]=0x00000000
ABS_OFFSET=0x28282828 result[0A]=0x00000000
ABS_OFFSET=0x2C2C2C2C result[0B]=0x00000000
ABS_OFFSET=0x30303030 result[0C]=0x00000000
ABS_OFFSET=0x34343434 result[0D]=0x00000000
ABS_OFFSET=0x38383838 result[0E]=0x00000000
ABS_OFFSET=0x3C3C3C3C result[0F]=0x00000000
ABS_OFFSET=0x40404040 result[10]=0x00000000
ABS_OFFSET=0x44444444 result[11]=0x00000000
ABS_OFFSET=0x48484848 result[12]=0x00000000
ABS_OFFSET=0x4C4C4C4C result[13]=0x00000000
ABS_OFFSET=0x50505050 result[14]=0x00000000
ABS_OFFSET=0x54545454 result[15]=0x00000000
ABS_OFFSET=0x58585858 result[16]=0x00000000
ABS_OFFSET=0x5C5C5C5C result[17]=0x00000000
ABS_OFFSET=0x60606060 result[18]=0x01000000
ABS_OFFSET=0x64646464 result[19]=0x01000011
ABS_OFFSET=0x68686868 result[1A]=0x01111111
ABS_OFFSET=0x6C6C6C6C result[1B]=0x01111111
ABS_OFFSET=0x70707070 result[1C]=0x11111111
ABS_OFFSET=0x74747474 result[1D]=0x11111111
ABS_OFFSET=0x78787878 result[1E]=0x11111111
ABS_OFFSET=0x7C7C7C7C result[1F]=0x11111111
Byte 0: (0x0c - 0x60), middle value:0x36
Byte 1: (0x10 - 0x60), middle value:0x38
Byte 2: (0x10 - 0x64), middle value:0x3a
Byte 3: (0x08 - 0x64), middle value:0x36
Byte 5: (0x14 - 0x64), middle value:0x3c
Byte 6: (0x08 - 0x5c), middle value:0x32
Byte 7: (0x18 - 0x6c), middle value:0x42
MMDC0 MPWRDLCTL = 0x363A3836,MMDC1 MPWRDLCTL = 0x42323C3A
MMDC registers updated from calibration
Write leveling calibration
MMDC_MPWLDECTRL0 ch0 (0x021b080c) = 0x001F0019
MMDC_MPWLDECTRL1 ch0 (0x021b0810) = 0x001F0023
MMDC_MPWLDECTRL0 ch1 (0x021b480c) = 0x0018001F
MMDC_MPWLDECTRL1 ch1 (0x021b4810) = 0x0006001F
Read DQS Gating calibration
MPDGCTRL0 PHY0 (0x021b083c) = 0x03300344
MPDGCTRL1 PHY0 (0x021b0840) = 0x0328031C
MPDGCTRL0 PHY1 (0x021b483c) = 0x03280338
MPDGCTRL1 PHY1 (0x021b4840) = 0x031C025C
Read calibration
MPRDDLCTL PHY0 (0x021b0848) = 0x3E322E34
MPRDDLCTL PHY1 (0x021b4848) = 0x34342E3E
Write calibration
MPWRDLCTL PHY0 (0x021b0850) = 0x363A3836
MPWRDLCTL PHY1 (0x021b4850) = 0x42323C3A
Success: DDR calibration completed!!!
============================================
DDR Stress Test (2.6.0)
Build: Aug 1 2017, 17:33:25
NXP Semiconductors.
DDR Stress Test Iteration 1
Current Temperature: 53
============================================
DDR Freq: 135 MHz
t0.1: data is addr test
Address of failure(step2): 0x10000000
Data was: 0x00000010
But pattern should match address
Error: failed to run stress test!!!
0x0 0x4 0x8 0xC
----------------------------------------------------------------------------------------------------------------
0x10000000: 0x00000010
memory read is done