imx6q: building linux image with both fb & x11 backends

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q: building linux image with both fb & x11 backends

921 次查看
pj0585
Contributor III

Hi,

I want to build the latest fsl-community-bsp image

(fsl-L3.14.28_1.0.0_ga). I can choose to build any one backend (fb, x11,

wayland or directfb). The libraries of the other backends are removed

or not built.

Is it possible to build the image for framebuffer (fb) backend but

also include libraries of the x11 backend ? If yes, can someone please point out to me how can I do this?

Regards, Pj

标签 (4)
标记 (3)
0 项奖励
回复
0 回复数