Hello,
we want to calibrate ddr3-RAM on a imx6-quad-board with "ddr-stress-test-mx6dq......." (for loading with JTAG).
Our imx6-board is running at the moment by booting a minimum imx6-config over JTAG
(using BDI3000 debugger). We are able to communicate to the board in this way. Also
it ist possible to load DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG elf-file
to address 0x00907000 in iRAM.
The TX/RX pad - configuration for UART1 was done (CSI0_DAT10/ALT3, CSI0_DAT11/ALT3).
Nevertheless we didn´t get any output on the serial UART1 console after starting the "ddr-stress-test"
with the command "go 0x0090700" in debugger-console.
We tried out to configure the UART1 (-registers) to match with RS232 and a baudrate of 115200Kbps.
But nothing will happen at the serial console.
I think we have to do the the configuration of the board in the imx6-config-file of the BDI3000 (like done
by u-boot when using usb-variante) to initialize basically for using "ddr-stress-test" .
Does anybody have a kind of user manual that decribes the main line we have to go to run the
"ddr-stress-test". I always found the things for u-boot/usb-actions.
Thank you very much for your help,
Tobi
解決済! 解決策の投稿を見る。
Hi Tobias
some reference boards configuration files one
can find in DDR_Stress_Tester_V1.0.3.zip
folder binary/scripts, documentation in
DDR_Stress_Tester_V1.0.3/Documentation.
Also recommended to look at
https://community.freescale.com/docs/DOC-101708
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor, hi Yur,
first of all: sorry for my late response and thank you for your quik help.
I found that interesting documents an have written an initialization script including
the configuration for the DDR3-Ram to setup imx6 while booting with BDI3000 and JTAG.
The result is the same as last week:
I can bring up the board with BDI3000-debugger
I can load than the ddr-stress-test (elf) file to 0x00907000
I can read back the values from the related registers, configured in the BDI3000-Script
I cannot start the ddr-stress-test by command "go 0x00907000" from BDI3000-debug-console successfully.
I think there is something other that i have to do for initializing the imx6.
What is the difference between the u-boot variant (.bin) and the JTAG-variant (.elf)?
What are the initialization steps I have to do on my own when I using JTAG (debugguer) instead of booting by u-boot
and serial downloader (usb-otg)?
Best regards and thanks for help.
Tobi
I am afraid You load the .elf file as binary image ("I can load than the ddr-stress-test (elf) file to 0x00907000").
"elf" is an object file, containing all the needed information for a loader and debugger. Therefore
it may be loaded without additional address as parameter. Address 0x00907000 should be used
for binary image. So, please try using the .bin file with start address or .elf - without any parameters,
if BDI3000 supports it.
Regards,
Yuri.
Tobias
BDI does support ELF. As Yuri mentioned it would load
to the address according to program header in the elf
file. After loading it, just dump the memory at this address
and compare it to that of ddr test program disassembly.
Also pay attention where the entry address of that
executable is. Load address and program entry can
be two different addresses.
Hope this helps
Sinan Akman
"DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG" can be loaded (via JTAG)
to internal RAM of the i.MX6 under serial downloader mode (BOOT_MODE[1:0] = 01).
It provides UART initialization. To run the test, DRAM memory must be initialized by
a JTAG script.
Regards,
Yuri.
Hi Tobias
some reference boards configuration files one
can find in DDR_Stress_Tester_V1.0.3.zip
folder binary/scripts, documentation in
DDR_Stress_Tester_V1.0.3/Documentation.
Also recommended to look at
https://community.freescale.com/docs/DOC-101708
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------