Hi,
I am stuck with audio recording through MIC_IN in sabreauto_6q with android 5.0.2
we have tried to record through android sound Recorder app and tinycap.
1) In SoundRecorder app the needle is not deflecting... but the recording continues and onplay it plays silence
2)In Tinycap it captures few frames but on playback its complete silence
| #tinycap /data/test.wav -d 1 -c2 | |
Capturing sample: 2 ch, 44100 hz, 16 bit
Captured 577536 frames
Please help us with fix or debussing on above issue.
Other observation is recording through LINE_IN is successful and audio playback is also working.
Details on make configuration:
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=5.0.2
TARGET_PRODUCT=sabreauto_6q
TARGET_BUILD_VARIANT=eng
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
TARGET_ARCH_VARIANT=armv7-a-neon
TARGET_CPU_VARIANT=cortex-a9
TARGET_2ND_ARCH=
TARGET_2ND_ARCH_VARIANT=
TARGET_2ND_CPU_VARIANT=
HOST_ARCH=x86_64
HOST_OS=linux
HOST_OS_EXTRA=Linux-3.13.0-32-generic-x86_64-with-Ubuntu-12.04-precise
HOST_BUILD_TYPE=release
BUILD_ID=1.0.0-ga-rc4
OUT_DIR=out
environment set :
# setenv bootargs 'console=ttymxc3,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=400M androidboot.console=ttymxc3 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled'
0 [cs42888audio ]: cs42888-audio - cs42888-audio
| | cs42888-audio |
| 1 [imxspdif | ]: imx-spdif - imx-spdif |
| | imx-spdif |
Thanks in advance ...