imx6q) How to test SPI, UART, CAN ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q) How to test SPI, UART, CAN ?

4,783 次查看
ktc7270
Contributor II

HI,

I want to test imx6q-sabresd. The device driver seems to be properly configured.

I want to know if there are test codes.

For example, the test code can transfer the spi data of the imx6 board to another board.

(The data received from the imx6 board can do something else through the test code.

Please help me.

ps. add questions.

标签 (2)
2 回复数

4,188 次查看
winy2014
Contributor II

Hi,

if users use i.MX6Q board designed by Forlinx, generally the related codes are provided.

Rgds,

Grace

0 项奖励
回复

4,185 次查看
igorpadykov
NXP Employee
NXP Employee

Hi kangta

for testing one can use unit tests described in Chapter 9 Unit Tests attached Linux Manual

imx-test
https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------