imx6q 5.0.2 U-boot 中mipi屏怎么配置

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q 5.0.2 U-boot 中mipi屏怎么配置

1,668 Views
ma519384084
Contributor I

现在我有一个项目需要使用mipi屏,但是我查看代码发现在u-boot中并没有mipi屏相关的部分,

我有参考Patch to support MIPI display(hx8369) in uboot for i.mx6DL/DQ SebreSD boards 里面的patch,但是我使用的代码是android 5.0.2版本的,在u-boot中与上面提供的patch存在很大的差异,整个代码流程都是完全不一样的,可以说完全不能依据patch中代码进行移植,不能知道该patch代码是什么意思,应该在什么时候执行,所以我在这里想请教是否有其他的patch或者说任何人有在新的版本中使用mipi屏?在u-boot中是怎么做的呢?

感谢各位,希望有人能够帮助我,谢谢!

Labels (1)
0 Kudos
2 Replies

1,171 Views
ma519384084
Contributor I

我想知道imx6q输出的mipi信号波形是什么样子的,数据脚以及clk脚各是什么样的,谁能告诉我?或者上传一个用示波器测量的图像给我?

0 Kudos

1,171 Views
ma519384084
Contributor I

我参考patch在uboot中移植了

power on and reset mipi_panel

mipi_clk enable

mipi_dsi enable controller

lcd init

DSI change to video mode

但是现在uboot只在mipi的数据脚有1.2V常高电平输出,并没有任何数据波形,并且clk只有200mV左右的长高输出。

而且在kernel中虽然mipi数据脚有1.2V数据波形出来,但是ckl也是只有200mV的波形输出。

anybody can help me?

0 Kudos