imx6duallite - fsl-image-machine-test -warning

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6duallite - fsl-image-machine-test -warning

916 次查看
shankovai
Contributor III

Hello Support team,

Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6dlsabresd"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:27de52e402ae000dfa502d52908cd6e6aef923ec"
meta-oe
meta-multimedia
meta-python = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-freescale = "HEAD:2fb1ce365338126aad365012ebb913b3e4a9f1be"
meta-freescale-3rdparty = "HEAD:de0eb1408150d77f9cce97c559f9a5a3c71e5d6c"
meta-freescale-distro = "HEAD:fc15f5003043da23212596be7366ae2547c308ad"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:5bc708f56575a878da17f2148e959c95d06cf8db"
meta-nxp-demo-experience = "HEAD:8fade3993b832ecd823771644f2a7b731f8f4527"
meta-chromium = "HEAD:d25d8ee98a656b2534d0eec6138ef264529fab4f"
meta-clang = "HEAD:85d956d95401479ca666139e31f662f60c156d5f"
meta-gnome
meta-networking
meta-filesystems = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-qt6 = "HEAD:b2894aad5c1aaa85f2f5c7b94391b7c51c39e555"
meta-virtualization = "HEAD:973c8d0964c6f40338857efe5b8009b2f647d485"

Initialising tasks: 100% |##############################################################################################################| Time: 0:00:06
Sstate summary: Wanted 2884 Local 0 Mirrors 0 Missed 2884 Current 0 (0% match, 0% complete)
NOTE: Executing Tasks
WARNING: sigma-dut-git-r0 do_populate_lic: QA Issue: sigma-dut: No generic license file exists for: BSD in any provider [license-exists]
WARNING: sudo-1.9.5p2-r0 do_populate_lic: QA Issue: sudo: No generic license file exists for: BSD in any provider [license-exists]
WARNING: wireless-tools-1_30.pre9-r0 do_populate_lic: QA Issue: wireless-tools: No generic license file exists for: BSD in any provider [license-exists]

while building the fsl-image-machine-test, above warning messages issued

how to solve the warning messages

thanks

 

0 项奖励
回复
1 回复

914 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello shankovai,

 

These are general messages of missing license you can pass the build with out notice.

 

Regards

0 项奖励
回复