imx6dq ipu/gpu dma DMA appears to be stuck at this address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dq ipu/gpu dma DMA appears to be stuck at this address

969 次查看
jiujinhong
Contributor IV

Hi,

We use kernel 4.1.15 AndroidN7.1.0 for customer. The project need to quick preview camera data when system booting if detect some hardware signal. Once not detect some hardware signal, it will display normal fb content(Android).

We have do some pressure test, if we do rapidly switch between camera deque/enque and normal fb, GPU will stack. should we need to add some delay to prevent ? please give some advice.

20190527_13:58:24][   32.448697] **************************
20190527_13:58:24][   32.452461] ***   GPU DRV CONFIG   ***
20190527_13:58:24][   32.456215] **************************
20190527_13:58:24][   32.468717] Galcore version 6.2.0.79565
20190527_13:58:24][   32.472562] Galcore options:
20190527_13:58:24][   32.475447]   irqLine           = 307
20190527_13:58:24][   32.479140]   registerMemBase   = 0x00130000
20190527_13:58:24][   32.483415]   registerMemSize   = 0x00004000
20190527_13:58:24][   32.487689]   irqLine2D         = 308
20190527_13:58:24][   32.491785]   registerMemBase2D = 0x00134000
20190527_13:58:24][   32.496064]   registerMemSize2D = 0x00004000
20190527_13:58:24][   32.500363]   irqLineVG         = 309
20190527_13:58:24][   32.504032]   registerMemBaseVG = 0x02204000
20190527_13:58:24][   32.508306]   registerMemSizeVG = 0x00004000
20190527_13:58:24][   32.512952]   contiguousSize    = 134217728
20190527_13:58:24][   32.517143]   contiguousBase    = 0x00000000
20190527_13:58:24][   32.521441]   bankSize          = 0x00000000
20190527_13:58:24][   32.525716]   fastClear         = -1
20190527_13:58:24][   32.529310]   compression       = -1
20190527_13:58:24][   32.532890]   signal            = 48
20190527_13:58:24][   32.536468]   powerManagement   = 1
20190527_13:58:24][   32.540454]   baseAddress       = 0x00000000
20190527_13:58:24][   32.544732]   physSize          = 0x80000000
20190527_13:58:24][   32.549031]   logFileSize       = 0 KB
20190527_13:58:24][   32.552871]   recovery          = 0
20190527_13:58:24][   32.556363]   stuckDump         = 0
20190527_13:58:24][   32.559873]   gpuProfiler       = 0
20190527_13:58:24][   32.563367]   irqs              = -1, -1, -1, -1, -1, -1,
20190527_13:58:24][   32.568983]   registerBases     = 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000,
20190527_13:58:24][   32.578763]   registerSizes     = 0x00000800, 0x00000800, 0x00000800, 0x00000800, 0x00000800, 0x00000800,
20190527_13:58:24][   32.588529]   chipIDs     = 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF, 0xFFFFFFFF,
20190527_13:58:24][   32.597789] Build options:
20190527_13:58:24][   32.600524]   gcdGPU_TIMEOUT    = 20000
20190527_13:58:24][   32.604365]   gcdGPU_2D_TIMEOUT = 20000
20190527_13:58:24][   32.608204]   gcdINTERRUPT_STATISTIC = 1
20190527_13:58:24][   32.612152] GPU[0](ChipModel=0x2000 ChipRevision=0x5108):
20190527_13:58:24][   32.619255] **************************
20190527_13:58:24][   32.623010] ***   GPU STATE DUMP   ***
20190527_13:58:24][   32.626762] **************************
20190527_13:58:24][   32.630531]   axi      = 0x00000050
20190527_13:58:24][   32.634025]   idle     = 0x7FFFFFFE
20190527_13:58:24][   32.637517]     FE not idle
20190527_13:58:24][   32.640330]   DMA appears to be stuck at this address:
20190527_13:58:24][   32.645474]     0xFFFF7978
20190527_13:58:24][   32.648185]   dmaLow   = 0xE286100C
20190527_13:58:24][   32.651693]   dmaHigh  = 0xE1A03000
20190527_13:58:24][   32.655187]   dmaState = 0x00000011
20190527_13:58:24][   32.658696]     command state       = 17 (PAR_WAITFIFO_ST)
20190527_13:58:24][   32.664189]     command DMA state   = 0 (CMD_IDLE_ST)
20190527_13:58:24][   32.669261]     command fetch state = 0 (FET_IDLE_ST)
20190527_13:58:24][   32.674318]     DMA request state   = 0 (REQ_IDLE_ST)
20190527_13:58:24][   32.679393]     cal state           = 0 (CAL_IDLE_ST)
20190527_13:58:24][   32.684451]     VE request state    = 0 (VER_IDLE_ST)
20190527_13:58:24][   32.689521]   Debug registers:
20190527_13:58:24][   32.692584]     RA[0] debug registers:
20190527_13:58:24][   32.696357]     [00] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.699821] bdstarcamera report uevent rvc_reverse_singal: REVERSE=SIGNAL
20190527_13:58:24][   32.711620]     [08] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.720099]     [10] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.728559]     [18] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.737034]     [20] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.745513]     [28] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.753988]     [30] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.762461]     [38] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.770937]     [40] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.779413]     [48] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.787875]     [50] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.796346]     [58] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.804822]     [60] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.813298]     [68] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.821774]     [70] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.830248]     [78] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.838724]     [80] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.847182]     [88] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.855653]     [90] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.864136]     [98] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.872612]     [A0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.881086]     [A8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.889561]     [B0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.892021] bdstarcamera report uevent rvc_reverse_singal: REVERSE=NO_SIGNAL
20190527_13:58:24][   32.905090]     [B8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.913574]     [C0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.922056]     [C8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.930537]     [D0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.939016]     [D8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.940074] bdstarcamera report uevent rvc_reverse_singal: REVERSE=SIGNAL
20190527_13:58:24][   32.954284]     [E0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.962764]     [E8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.971242]     [F0] 00000000 00000000 00000000 00000000 039F0000 02070000 81AA8000 00000000
20190527_13:58:24][   32.979717]     [F8] 00000000 00000000 00000000 00000000 12344321 12344321 12344321 12344321
20190527_13:58:24][   32.988162]     TX[0] debug registers:
20190527_13:58:24][   32.991952]     [00] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.000429]     [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.008903]     [10] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.017360]     [18] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.025833]     [20] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.034309]     [28] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.042783]     [30] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.051257]     [38] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.059758]     [40] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.068218]     [48] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.076695]     [50] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.085170]     [58] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.093644]     [60] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.102124]     [68] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.110601]     [70] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.119087]     [78] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:24][   33.127532]     FE[0] debug registers:
20190527_13:58:24][   33.131319]     [00] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.139795]     [08] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A0 BABEF00D
20190527_13:58:24][   33.148253]     [10] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.156724]     [18] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A1 BABEF00D
20190527_13:58:24][   33.165196]     [20] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.173668]     [28] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A2 BABEF00D
20190527_13:58:24][   33.182143]     [30] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.190615]     [38] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A3 BABEF00D
20190527_13:58:24][   33.199090]     [40] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.207548]     [48] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A4 BABEF00D
20190527_13:58:24][   33.216022]     [50] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.224497]     [58] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A5 BABEF00D
20190527_13:58:24][   33.228699] bdstarcamera report uevent rvc_reverse_singal: REVERSE=NO_SIGNAL
20190527_13:58:24][   33.240029]     [60] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.248490]     [68] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A6 BABEF00D
20190527_13:58:24][   33.256967]     [70] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.265446]     [78] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A7 BABEF00D
20190527_13:58:24][   33.273925]     [80] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.282402]     [88] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000A8 BABEF00D
20190527_13:58:24][   33.290875]     [90] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.299351]     [98] 0000000E 00000000 00000000 00000000 00000000 BFFFE801 000000A9 BABEF00D
20190527_13:58:24][   33.307810]     [A0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.316284]     [A8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AA BABEF00D
20190527_13:58:24][   33.324761]     [B0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.333238]     [B8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AB BABEF00D
20190527_13:58:24][   33.341718]     [C0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.350195]     [C8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AC BABEF00D
20190527_13:58:24][   33.358656]     [D0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.367134]     [D8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AD BABEF00D
20190527_13:58:24][   33.375612]     [E0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:24][   33.384100]     [E8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AE BABEF00D
20190527_13:58:25][   33.392582]     [F0] FFFF7980 E88D0180 E58D4008 00000250 0000072F 0000000C 00009571 00007245
20190527_13:58:25][   33.401059]     [F8] 0000000E 00000000 00000000 00000000 00000000 A3409A4D 000000AF BABEF00D
20190527_13:58:25][   33.409522]     PE[0] debug registers:
20190527_13:58:25][   33.413296]     [00] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.421773]     [08] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.430253]     [10] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.438733]     [18] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.447193]     [20] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.455670]     [28] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.464151]     [30] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.472628]     [38] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.481103]     [40] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.489583]     [48] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.498042]     [50] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.506520]     [58] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.514998]     [60] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.523475]     [68] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.531955]     [70] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.540430]     [78] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.548910]     [80] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.557370]     [88] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.565846]     [90] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.574328]     [98] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.582807]     [A0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.591285]     [A8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.599759]     [B0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.608221]     [B8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.616696]     [C0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.625176]     [C8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.633654]     [D0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.642140]     [D8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.650620]     [E0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.659099]     [E8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.667560]     [F0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.676037]     [F8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.684499]     PE[1] debug registers:
20190527_13:58:25][   33.688272]     [00] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.696748]     [08] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.705227]     [10] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.713706]     [18] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.722186]     [20] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.730662]     [28] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.739140]     [30] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.747599]     [38] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.756073]     [40] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.764554]     [48] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.773032]     [50] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.781509]     [58] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.789982]     [60] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.798443]     [68] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.806916]     [70] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.815395]     [78] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.823873]     [80] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.832350]     [88] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.840824]     [90] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.849302]     [98] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.857763]     [A0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.866242]     [A8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.874719]     [B0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.883194]     [B8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.891670]     [C0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.900153]     [C8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.908621]     [D0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.917099]     [D8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.925577]     [E0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.934056]     [E8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.942534]     [F0] 00000000 00000000 00000000 00000000 A0000000 ABC00000 BC000000 CDE00000
20190527_13:58:25][   33.951010]     [F8] D04045C0 204045C0 0D863284 00000000 BABEF00D BABEF00D BABEF00D BABEF00D
20190527_13:58:25][   33.959473]     DE[0] debug registers:
20190527_13:58:25][   33.963246]     [00] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   33.971723]     [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   33.980198]     [10] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   33.988657]     [18] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   33.997160]     [20] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.005641]     [28] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.014120]     [30] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.022597]     [38] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.031074]     [40] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.039553]     [48] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.048013]     [50] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.056485]     [58] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.064963]     [60] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.073439]     [68] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.081917]     [70] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.090391]     [78] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.098867]     [80] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.107328]     [88] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.115805]     [90] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.124283]     [98] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.132760]     [A0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.141238]     [A8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.149714]     [B0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.158175]     [B8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.166660]     [C0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.175142]     [C8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.183620]     [D0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.192100]     [D8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.200573]     [E0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.209052]     [E8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.217513]     [F0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.225989]     [F8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.234453]     SH[0] debug registers:
20190527_13:58:25][   34.238229]     [00] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.246707]     [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.255183]     [10] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.263658]     [18] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.272137]     [20] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.280613]     [28] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.289089]     [30] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.297550]     [38] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.306024]     [40] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.314500]     [48] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.322979]     [50] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.331458]     [58] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.339934]     [60] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.348395]     [68] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.356868]     [70] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.365343]     [78] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:25][   34.373819]     [80] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:25][   34.382299]     [88] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.390774]     [90] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.399249]     [98] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.407709]     [A0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.416184]     [A8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.424669]     [B0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.433148]     [B8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.441629]     [C0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.450103]     [C8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.458564]     [D0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.467041]     [D8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.475518]     [E0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.483995]     [E8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.492474]     [F0] 80FFE00B 555F0000 00000005 00080220 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.500948]     [F8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 DEADBEEF
20190527_13:58:26][   34.509410]     PA[0] debug registers:
20190527_13:58:26][   34.513183]     [00] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.521660]     [08] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.530139]     [10] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.538600]     [18] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.547078]     [20] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.555554]     [28] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.564031]     [30] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.572508]     [38] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.580982]     [40] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.589461]     [48] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.597922]     [50] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.606398]     [58] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.614876]     [60] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.623354]     [68] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.631831]     [70] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.640307]     [78] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.648788]     [80] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.657249]     [88] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.665727]     [90] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.674204]     [98] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.682692]     [A0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.691173]     [A8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.699647]     [B0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.708108]     [B8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.716583]     [C0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.725063]     [C8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.733541]     [D0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.742022]     [D8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.750498]     [E0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.758975]     [E8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.767435]     [F0] 800001FF 00280000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:26][   34.775909]     [F8] 00000000 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA 0000AAAA
20190527_13:58:26][   34.784373]     SE[0] debug registers:
20190527_13:58:26][   34.788148]     [00] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.796627]     [08] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.805103]     [10] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.813581]     [18] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.822059]     [20] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.830535]     [28] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.839012]     [30] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.847471]     [38] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.855947]     [40] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.864424]     [48] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.872900]     [50] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.881378]     [58] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.889854]     [60] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.898315]     [68] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.906791]     [70] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.915269]     [78] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.923745]     [80] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.932222]     [88] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.940709]     [90] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.949191]     [98] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.957650]     [A0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.966128]     [A8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.974606]     [B0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.983085]     [B8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   34.991563]     [C0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.000037]     [C8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.008498]     [D0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.016972]     [D8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.025451]     [E0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.033931]     [E8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.042407]     [F0] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.050880]     [F8] 00000003 00000003 00000003 00000003 00000003 00000003 00000003 00000003
20190527_13:58:26][   35.059346]     MC[0] debug registers:
20190527_13:58:26][   35.063122]     [00] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.071599]     [08] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.080077]     [10] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.088537]     [18] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.097015]     [20] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.105490]     [28] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.113966]     [30] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.122445]     [38] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.130920]     [40] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.139397]     [48] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.147857]     [50] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.156331]     [58] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.164808]     [60] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.173287]     [68] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.181766]     [70] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.190243]     [78] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.198727]     [80] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.207189]     [88] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.215667]     [90] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.224145]     [98] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.232622]     [A0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.241099]     [A8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.249576]     [B0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.258037]     [B8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.266514]     [C0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.274992]     [C8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.283471]     [D0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.291949]     [D8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.300424]     [E0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.308904]     [E8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.317365]     [F0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.325842]     [F8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.334302]     MC[1] debug registers:
20190527_13:58:26][   35.338077]     [00] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:26][   35.346554]     [08] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.355028]     [10] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.363508]     [18] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.371987]     [20] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.380467]     [28] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.388944]     [30] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.397405]     [38] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.405879]     [40] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.414355]     [48] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.422835]     [50] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.431314]     [58] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.439788]     [60] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.448249]     [68] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.456724]     [70] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.465210]     [78] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.473687]     [80] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.482167]     [88] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.490645]     [90] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.499124]     [98] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.507586]     [A0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.516064]     [A8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.524540]     [B0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.533016]     [B8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.541496]     [C0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.549974]     [C8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.558435]     [D0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.566914]     [D8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.575393]     [E0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.583873]     [E8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.592350]     [F0] 00000000 00000000 00000000 00000000 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.600824]     [F8] 12345678 12345678 12345678 12345678 12345678 12345678 12345678 12345678
20190527_13:58:27][   35.609289]     HI[0] debug registers:
20190527_13:58:27][   35.613065]     [00] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.621542]     [08] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.630019]     [10] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.638480]     [18] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.646957] AAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.663910]     [30] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.672389]     [38] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.680872]     [40] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27]
20190527_13:58:27][   35.689358]     [48] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27]130|s401:/ # [   35.697986]     [50] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.707589]     [58] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.716071]     [60] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.724562]     [68] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.733044]     [70] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.741524]     [78] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.750000]     [80] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.758460]     [88] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.766937]     [90] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.775416]     [98] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.783893]     [A0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.792368]     [A8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.800842]     [B0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.809322]     [B8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.817782]     [C0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.826260]     [C8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.834737]     [D0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.843214]     [D8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.851693]     [E0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.860167]     [E8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.868627]     [F0] 00000000 00000000 00000000 AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.877104]     [F8] AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA AAAAAAAA
20190527_13:58:27][   35.885566]     TPG[1] debug registers:
20190527_13:58:27][   35.889442]     [80] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.897901]     [88] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.906377]     [90] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.914856]     [98] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.923318]     TFB[1] debug registers:
20190527_13:58:27][   35.927179]     [A0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.935654]     [A8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.944135]     [B0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.952612]     [B8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.961073]     USC[1] debug registers:
20190527_13:58:27][   35.964934]     [C0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.973411]     [C8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.981898]     [D0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.990377]     [D8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   35.998856]     [E0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.007316]     [E8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.015790]     [F0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.024267]     [F8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.032731]     L2[0] debug registers:
20190527_13:58:27][   36.036505]     [00] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.044984]     [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.053462]     [10] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.061942]     [18] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.070420]     [20] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.078896]     [28] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.087358]     [30] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.095834]     [38] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.104313]     [40] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.112790]     [48] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.121265]     [50] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.129742]     [58] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.138202]     [60] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.146677]     [68] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.155155]     [70] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.163634]     [78] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.172109]     [80] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.180585]     [88] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.189064]     [90] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.197523]     [98] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.206000]     [A0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.214480]     [A8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.222955]     [B0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.231433]     [B8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.239920]     [C0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.248383]     [C8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.256861]     [D0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.265335]     [D8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.273813]     [E0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.282290]     [E8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.290766]     [F0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.299244]     [F8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.307688]     BLT[0] debug registers:
20190527_13:58:27][   36.311565]     [00] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.320041]     [08] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.328500]     [10] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.336977]     [18] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.345454]     [20] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.353929]     [28] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.362408]     [30] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.370883]     [38] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.379360]     [40] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:27][   36.387820]     [48] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.396296]     [50] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.404769]     [58] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.413246]     [60] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.421722]     [68] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.430195]     [70] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.438654]     [78] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.447128]     [80] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.455606]     [88] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.464081]     [90] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.472555]     [98] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.481031]     [A0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.489511]     [A8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][  0000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.514941]     [C0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.523418]     [C8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.531893]     [D0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.540366]     [D8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28]
20190527_13:58:28][   36.548844]     [E0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28]130|s401:/ # [   36.557458]     [E8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.567056]     [F0] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.575532]     [F8] 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.583995]     Other Registers[0]:
20190527_13:58:28][   36.587493]       [0x0040] 0x00000467
20190527_13:58:28][   36.591180]       [0x0044] 0x00000000
20190527_13:58:28][   36.594851]       [0x004C] 0x00000000
20190527_13:58:28][   36.598519]       [0x0050] 0x00000000
20190527_13:58:28][   36.602204]       [0x0054] 0x00000000
20190527_13:58:28][   36.605875]       [0x0058] 0x00000467
20190527_13:58:28][   36.609559]       [0x005C] 0x00000141
20190527_13:58:28][   36.613230]       [0x0060] 0x00000141
20190527_13:58:28][   36.616897]       [0x043C] 0x00000000
20190527_13:58:28][   36.620582]       [0x0440] 0x00000000
20190527_13:58:28][   36.624252]       [0x0444] 0x00000000
20190527_13:58:28][   36.627919]       [0x0414] 0x3C000000
20190527_13:58:28][   36.631605]       [0x0100] 0x00140021
20190527_13:58:28][   36.635274]     Other Registers[1]:
20190527_13:58:28][   36.638787]       [0x0040] 0x00000462
20190527_13:58:28][   36.642459]       [0x0044] 0x00000000
20190527_13:58:28][   36.646128]       [0x004C] 0x00000000
20190527_13:58:28][   36.649813]       [0x0050] 0x00000000
20190527_13:58:28][   36.653484]       [0x0054] 0x00000000
20190527_13:58:28][   36.657152]       [0x0058] 0x00000462
20190527_13:58:28][   36.660835]       [0x005C] 0x00000141
20190527_13:58:28][   36.664504]       [0x0060] 0x00000141
20190527_13:58:28][   36.668172]       [0x043C] 0x00000000
20190527_13:58:28][   36.671858]       [0x0440] 0x00000000
20190527_13:58:28][   36.675528]       [0x0444] 0x00000000
20190527_13:58:28][   36.679211]       [0x0414] 0x3C000000
20190527_13:58:28][   36.682880]       [0x0100] 0x00140021
20190527_13:58:28][   36.686585]     Link stack:
20190527_13:58:28][   36.689461]       [0x00] 0xA3409A4D [0x01] 0xA3409A4D [0x02] 0xA3409A4D [0x03] 0xA3409A4D
20190527_13:58:28][   36.697648]       [0x04] 0xA3409A4D [0x05] 0xA3409A4D [0x06] 0xA3409A4D [0x07] 0xA3409A4D
20190527_13:58:28][   36.705849]       [0x08] 0xA3409A4D [0x09] 0xA3409A4D [0x0A] 0xA3409A4D [0x0B] 0xA3409A4D
20190527_13:58:28][   36.714049]       [0x0C] 0xA3409A4D [0x0D] 0xA3409A4D [0x0E] 0xBFFFE801 [0x0F] 0xA3409A4D
20190527_13:58:28][   36.722388]   PRE_STACK:
20190527_13:58:28][   36.724932]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.732961]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.740988]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.749017]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.757028]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.765062]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.773093]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.781122]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.789333]   CMD_STACK:
20190527_13:58:28][   36.791877]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.70 00000000
20190527_13:58:28][   36.823967]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.831996]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.840020]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.848032]     00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
20190527_13:58:28][   36.856055]   LINK_STACK:
20190527_13:58:28]
20190527_13:58:28][   36.858700]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.866876]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.874904]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28]130|s401:/ # [   36.882934]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.892082]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.900111]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.908123]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.916150]     000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB 000000AB
20190527_13:58:28][   36.924176] **************************
20190527_13:58:28][   36.927932] *****   SW COUNTERS  *****
20190527_13:58:28][   36.931703] **************************
20190527_13:58:28][   36.935461]     Execute Count = 0x00000008
20190527_13:58:28][   36.939577]     Execute Addr  = 0x1A04D268
20190527_13:58:28][   36.943683]     End     Addr  = 0x1A04D258
20190527_13:58:28][   36.947788] CPU: 2 PID: 6 Comm: kworker/u8:0 Not tainted 4.1.15 #1
20190527_13:58:28][   36.953993] Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
20190527_13:58:28][   36.960558] Workqueue: galcore workqueue _TimerFunction
20190527_13:58:28][   36.965828] [<c010ff78>] (unwind_backtrace) from [<c010c0e4>] (show_stack+0x10/0x14)
20190527_13:58:28][   36.973614] [<c010c0e4>] (show_stack) from [<c08c5518>] (dump_stack+0x8c/0xcc)
20190527_13:58:28][   36.980879] [<c08c5518>] (dump_stack) from [<c05d8804>] (gckOS_DumpCallStack+0x8/0x10)
20190527_13:58:28][   36.988835] [<c05d8804>] (gckOS_DumpCallStack) from [<c05fd918>] (gckHARDWARE_DumpGPUState+0x7e8/0x9d8)
20190527_13:58:28][   36.998246] [<c05fd918>] (gckHARDWARE_DumpGPUState) from [<c05de238>] (_DumpState+0x10/0x2c)
20190527_13:58:28][   37.006715] [<c05de238>] (_DumpState) from [<c05deeb8>] (gckKERNEL_Recovery+0x110/0x14c)
20190527_13:58:28][   37.014837] [<c05deeb8>] (gckKERNEL_Recovery) from [<c05df08c>] (_MonitorTimerFunction+0x198/0x1a4)
20190527_13:58:28][   37.023926] [<c05df08c>] (_MonitorTimerFunction) from [<c0141508>] (process_one_work+0x144/0x484)
20190527_13:58:28][   37.032831] [<c0141508>] (process_one_work) from [<c0141bfc>] (worker_thread+0x4c/0x4f0)
20190527_13:58:28][   37.040954] [<c0141bfc>] (worker_thread) from [<c0147078>] (kthread+0xdc/0xf4)
20190527_13:58:28][   37.048195] [<c0147078>] (kthread) from [<c0108228>] (ret_from_fork+0x14/0x2c)
20190527_13:58:28][   37.055444] **************************
20190527_13:58:28][   37.059215] **** COMMAND BUF DUMP ****
20190527_13:58:28][   37.062970] **************************
20190527_13:58:28][   37.066723]   Submitted commit stamp = 8
20190527_13:58:28][   37.070668]   Executed commit stamp  = 4
20190527_13:58:28][   37.074600] DMA Address 0xFFFF7978, memory around:

标签 (4)
0 项奖励
3 回复数

810 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiu

to narrow down issue (if this is not caused by custom board) one can try

to test ddr memory

i.MX6/7 DDR Stress Test Tool V3.00 

and try to test on i.MX6Q Sabre SD reference board with Android 7.1 Demo Image

Demo Images - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

810 次查看
jiujinhong
Contributor IV

Hi,

our board has passed DDR stresstest tool.

about the case, We need official explain about "DMA stuck", please tell us WHY?  We need it so that we can optimize our driver code why it some time GPU stuck, meanwhile, please don't tell us that we need to update our bsp to latest gpu driver, our project is in the end of development, we have no enough time to upgrade even if full of other risk.

0 项奖励

810 次查看
igorpadykov
NXP Employee
NXP Employee

please try to reproduce that on i.MX6Q Sabre SD reference board with Android 7.1 Demo Image

Demo Images - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite

Best regards
igor

0 项奖励