imx6dp 关于gplay 的源码中有没有接口能将播放的视频指定到FB0上。#gstreamer#framebuffer#gplay-1.0#imx6dp
Hi cao jian,
You can specify the framebuffer using --video-sink option.You can check below link for more options:
Ubuntu Manpage: gst-play-1.0 - Simple command line playback testing tool
Regards,
Karan Gajjar
In our default BSP use the FB0. You need to set the display first in u-boot.
For play video, you can use the command like "gplay-1.0 test.mp4" or "gst-launch-1.0 playbin file=uri:///", for alpha blending, you can set alpha value in the gstreamer, use the paramter like "alpha=xx" in the gstreamer command, fb0 is BG for alpha blending
Could you tell us which version of BSP are you using?