imx6dl uboot2009 fastboot can not boot up!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6dl uboot2009 fastboot can not boot up!!

跳至解决方案
1,485 次查看
linw
Contributor I

In imx6dl board uboot version is 2009, fastboot flash bootloader u-boot.bin to the emmc, but can't boot up!!

MMC write: dev # 3, block # 16384, count 8688 ... 8688 blocks write: OK

Writing 'boot' DONE!

send: OKAY                                                                                                                      

cmdbuf: reboot                                                                                                                  

send: OKAY                                                                                                                      

resetting ...                     //////////hanging here!!!                                                                                              

                                                                                                                                

                                                                                                                                

U-Boot 2009.08-dirty (Sep 28 2015 - 18:58:32)

标签 (4)
0 项奖励
回复
1 解答
1,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lin

please check below link for eMMC fast boot

imx6q eMMC Fast Boot, someone using it can help ?

also please verify that uboot flash_header.S was changed

with DDR settings found from DDR test for this board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,280 次查看
linw
Contributor I

All I wanna do is use fastboot tool flash the image to emmc. I use MGTool flash the u-boot.bin to emmc it can boot up,but fastboot cmd can not. don't know why??

0 项奖励
回复
1,281 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lin

please check below link for eMMC fast boot

imx6q eMMC Fast Boot, someone using it can help ?

also please verify that uboot flash_header.S was changed

with DDR settings found from DDR test for this board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复