imx6dl sabresd board build Android8.0 ethernet can not work on giga switch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl sabresd board build Android8.0 ethernet can not work on giga switch

794 次查看
james_wu1
Contributor I

We use imx6dl sabresd board and build Android8.0

We just build with nxp BSP source code(no more modify the code) and run on sabresd demo board.

When Ethernet port connect to Gita switch appear "fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off"  (network can not work)

When Ethernet port connect to10/100 switch appear "fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx" (network can work).

please help.

thank you.

标签 (1)
0 项奖励
回复
0 回复数