imx6dl gstreamer 1.0 playbin fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6dl gstreamer 1.0 playbin fails

跳至解决方案
4,384 次查看
jefflancaster
Contributor I

I am using imx6dl, Linux kernel 3.14 (yocto-dizzy), gstreamer 1.0, gstreamer-imx libraries, and all the necessary gst-plugins.

Problem: I can't get playbin to use the imx vpu library components, specifically the imxvpuenc_h264.

root@imx6dl-slimline:~# gst-launch-1.0 playbin uri=file:///home/root/2015-08-23_12h17m15s.mp4

Setting pipeline to PAUSED ...

Pipeline is PREROLLING ...

Missing element: H.264 decoder <<<<<<<<<<<<<<<<<<< PROBLEM !!!!

WARNING: from element /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: No decoder available for type 'video/x-h264, stream-format=(string)avc, alignment=(string)au, level=(string)3.1, profile=(string)high, codec_data=(buffer)0164401fffe100182764401fac2c6a014016e9a828302a000007d20001d4c02801000528ee0462c0, width=(int)1280, height=(int)720, framerate=(fraction)5000/501, pixel-aspect-ratio=(fraction)1/1'.

Additional debug info:

/home/jeff/git/slimline/build/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.4.1-r0/gst-plugins-base-1.4.1/gst/playback/gsturidecodebin.c(939): unknown_type_cb (): /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0

ERROR: from element /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0: Your GStreamer installation is missing a plug-in.

Additional debug info:

/home/jeff/git/slimline/build/tmp/work/cortexa9hf-vfp-neon-mx6qdl-poky-linux-gnueabi/gstreamer1.0-plugins-base/1.4.1-r0/gst-plugins-base-1.4.1/gst/playback/gsturidecodebin.c(990): no_more_pads_full (): /GstPlayBin:playbin0/GstURIDecodeBin:uridecodebin0:

no suitable plugins found

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

Freeing pipeline ...

I built and installed the gstreamer-imx libraries:

root@imx6dl-slimline:~# gst-inspect-1.0 | grep imx

imxvpu:  imxvpudec: Freescale VPU video decoder

imxvpu:  imxvpuenc_h263: Freescale VPU h.263 video encoder

imxvpu:  imxvpuenc_h264: Freescale VPU h.264 video encoder

imxvpu:  imxvpuenc_mpeg4: Freescale VPU MPEG-4 video encoder

imxvpu:  imxvpuenc_mjpeg: Freescale VPU motion JPEG video encoder

imxpxp:  imxpxpvideosink: Freescale PxP video sink

imxpxp:  imxpxpvideotransform: Freescale PxP video transform

imxaudio:  imxuniaudiodec: Freescale i.MX uniaudio decoder

imxaudio:  imxmp3audioenc: Freescale i.MX MP3 encoder

imxeglvivsink:  imxeglvivsink: Freescale EGL video sink

imxg2d:  imxg2dvideosink: Freescale G2D video sink

imxg2d:  imxg2dvideotransform: Freescale G2D video transform

imxg2d:  imxg2dcompositor: Freescale G2D video compositor

imxipu:  imxipuvideotransform: Freescale IPU video transform

imxipu:  imxipuvideosink: Freescale IPU video sink

imxipu:  imxipucompositor: Freescale IPU video compositor

imxv4l2videosrc:  imxv4l2videosrc: V4L2 CSI Video Source

标签 (5)
0 项奖励
回复
1 解答
3,028 次查看
joanxie
NXP TechSupport
NXP TechSupport

great, so gstreamer works fine totally, right? if yes, pls close this thread.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,028 次查看
jefflancaster
Contributor I

I didn't have the h264parse plugin installed in my build. Now it works fine.

0 项奖励
回复
3,029 次查看
joanxie
NXP TechSupport
NXP TechSupport

great, so gstreamer works fine totally, right? if yes, pls close this thread.

0 项奖励
回复
3,028 次查看
joanxie
NXP TechSupport
NXP TechSupport

if you use the command "gst-inspect-1.0 | grep playbin", what can you get? any error message?

and what image do you use? demo image or built by customer?

0 项奖励
回复