imx6dl external asynchronous SRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl external asynchronous SRAM

1,791 次查看
shashikanthirem
Contributor III

Hi All,

I have one doubt  on imx6dl platform

do we have  EIM_LBA polarity configurable ?

Note:

as EIM_LBA pin is connected to external SRAM latch pin which is a active high signal, 

Ideally we should have put a NOT gate between EIM_LBA  and Latch Enable pin of ext SRAM , as this EIM_LBA is active low, make ADDR to get latch this pin will be ZERO, but our ext SRAM latch pin is active HIGH, which does not work at all, 

guys any input on work around on software without making hardware change.

标签 (2)
标记 (3)
0 项奖励
回复
2 回复数

1,742 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shashikant

>do we have  EIM_LBA polarity configurable ?

unfortunately not, polarity is not configurable.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,742 次查看
shashikanthirem
Contributor III

ok so this has to be a hardware change in  my scenario

0 项奖励
回复