Our application of scene must use 1024x768 for HDMI. But i
found that imx6dl's HDMI transmitter have a problem to output in
1024x768. Others is ok, such as 1280x1024, 800x600.
So, does the imx6dl HDMI support 1024x768 output?
board: Ours
cpu: IMX6DL
BSP: L3.0.35_4.1.0_130816_source.tar.gz
Hi Peterchan,
Thank you. The issue has been fixed. Our display device doesn't support 1024x768.
So, it will be ok to add an default timing for 1024x768 to mode list after got HDMI edid.
Hi xiaofei,
If your problem have solved, would you please help close this thread by clicking the Correct Answer or Helpful Answer button. Thanks a lot.
Have a great day
Best Regards
Dan
Hi Xiaofei,
You can refer to the thread iMX6 HDMI output 1366x768 resolution.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The kernel restricts it, if I recall correctly.
You can take a look in Boundary Devices' kernel tree as they have a patch to address it and base on that.
Hi Otavio,
Thank you very much. I don't know how to get kernel tree or patch from Boundary Devices. Could you show me?
Best wishes,
Xiaofei