imx6dl CPU frequence could not be 996000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6dl CPU frequence could not be 996000

1,138件の閲覧回数
Mihan
Contributor IV

Hi all

I find the CPU frequence could not be 996000, here is the cpu-info:

cpufreq-info
cpufrequtils 008: cpufreq-info (C) Dominik Brodowski 2004-2009
Report errors and bugs to cpufreq@vger.kernel.org, please.
analyzing CPU 0:
driver: imx6q-cpufreq
CPUs which run at the same hardware frequency: 0 1
CPUs which need to have their frequency coordinated by software: 0 1
maximum transition latency: 65.0 us.
hardware limits: 396 MHz - 792 MHz
available frequency steps: 396 MHz, 792 MHz
available cpufreq governors: interactive, conservative, userspace, powersave, ondemand, performance
current policy: frequency should be within 396 MHz and 792 MHz.
The governor "performance" may decide which speed to use
within this range.
current CPU frequency is 792 MHz (asserted by call to hardware).
cpufreq stats: 396 MHz:1.15%, 792 MHz:98.85% (756)
analyzing CPU 1:
driver: imx6q-cpufreq
CPUs which run at the same hardware frequency: 0 1
CPUs which need to have their frequency coordinated by software: 0 1
maximum transition latency: 65.0 us.
hardware limits: 396 MHz - 792 MHz
available frequency steps: 396 MHz, 792 MHz
available cpufreq governors: interactive, conservative, userspace, powersave, ondemand, performance
current policy: frequency should be within 396 MHz and 792 MHz.
The governor "performance" may decide which speed to use
within this range.
current CPU frequency is 792 MHz (asserted by call to hardware).
cpufreq stats: 396 MHz:1.15%, 792 MHz:98.85% (756)

But the device tree has defined the 996Mhz:

cpus {
#address-cells = <1>;
#size-cells = <0>;

cpu0: cpu@0 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = <0>;
next-level-cache = <&L2>;
operating-points = <
/* kHz uV */
996000 1250000
792000 1175000
396000 1150000
>;
fsl,soc-operating-points = <
/* ARM kHz SOC-PU uV */
996000 1175000
792000 1175000
396000 1175000
>;
clock-latency = <61036>; /* two CLK32 periods */
clocks = <&clks IMX6QDL_CLK_ARM>,
<&clks IMX6QDL_CLK_PLL2_PFD2_396M>,
<&clks IMX6QDL_CLK_STEP>,
<&clks IMX6QDL_CLK_PLL1_SW>,
<&clks IMX6QDL_CLK_PLL1_SYS>,
<&clks IMX6QDL_CLK_PLL1>,
<&clks IMX6QDL_PLL1_BYPASS>,
<&clks IMX6QDL_PLL1_BYPASS_SRC>;
clock-names = "arm", "pll2_pfd2_396m", "step",
"pll1_sw", "pll1_sys", "pll1",
"pll1_bypass", "pll1_bypass_src";
arm-supply = <&reg_arm>;
pu-supply = <&reg_pu>;
soc-supply = <&reg_soc>;
};

cpu@1 {
compatible = "arm,cortex-a9";
device_type = "cpu";
reg = <1>;
next-level-cache = <&L2>;
};

Is there any condition for that, on hardware or kernel configure?

 

Best regards

Mihan

0 件の賞賛
返信
1 返信

1,132件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi  铭恒

 

some parts like industrial work up to 800MHz only, software can read fuse "Temperature Grade",

Table 1. Example Orderable Part Numbers  i.MX 6Solo/6DualLite Applications Processors for Industrial Products

 

Best regards
igor

0 件の賞賛
返信