imx6ULL WDOG1_ANY signal = same as imx6SoloX WDOG1_ANY?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ULL WDOG1_ANY signal = same as imx6SoloX WDOG1_ANY?

Jump to solution
776 Views
r_veens
Contributor III

Hey,

We are looking at the watchdogs of the imx6ull and we find that the first instance (WDOG1) has an extra signal named WDOG1_ANY.

The imx6ULL RM does not say anything about this external signal.

 

This post mentions that the signal is the logical AND of all the WDOG_B signals of all watchdog instances:

https://community.nxp.com/t5/i-MX-Processors/About-WDOG1-ANY-signal-of-i-MX6SoloX/td-p/459008 

 

My question is, is this true as well for the imx6ull?

 

I see that the IMX6soloX RM has since been updated:

r_veens_0-1611339647807.png

 

But this is not the case for the IMX6ULL:

r_veens_1-1611339679142.png

 

Would someone be able to clarify this? Thanks in advance.

Labels (2)
0 Kudos
Reply
1 Solution
768 Views
igorpadykov
NXP Employee
NXP Employee

Hi r_veens

 

yes this is also true for the imx6ull.

 

Best regards
igor

 

 

View solution in original post

0 Kudos
Reply
1 Reply
769 Views
igorpadykov
NXP Employee
NXP Employee

Hi r_veens

 

yes this is also true for the imx6ull.

 

Best regards
igor

 

 

0 Kudos
Reply