imx6ULL CAN Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ULL CAN Connection

498 次查看
soumyaks
Contributor II

Hi All,

I am using imx6.ULL EVK board. There is a CAN connector on the board which has pins for both CAN0(L/H) and CAN1(L/H).

I want to do a loop back from CAN0 to CAN1. How should I connect these pins? Is it enough if I just wire it up from L-L and H-H of Can0-Can1 respectively? There was a continuity seen in the other pins when I do that.

Is there a cable which can be procured anywhere particularly for this EVK?

Any leads will be of atmost help.

Thanks,

Soumya

标签 (1)
0 项奖励
1 回复

334 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Soumya

I believe you are right, for loop back just connect L-L and H-H of Can0-Can1 respectively.

For test one can use imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励