Hello,
Does i.MX6 Ultralite support any kind of hardware acceleration of Ethernet switching on its two Ethernet interfaces? And if yes how to enable it?
If I compile and use the Linux Ethernet bridge module, then system load at maximum 100Mbit throughput is approximately 50% when 1500 byte packets are used. If smaller packets are used then the system load goes easily to 100%.
Platform used: IMX6UL-EVK
Part: PCIMX6G2CVM05AA
Kernel/BSP: Linux imx6ulevk 3.14.38-6UL_ga+ge4944a5 (compiled with bridge module)
Traffic generator: iperf -s / iperf -c
Load test: sar -u 5 100
Thank you very much beforehand.
Vladislav
已解决! 转到解答。
i.MX6UL Ethernet controllers offer certain acceleration to the OS
network stack, but these features mostly offload above-L2 tasks, such
as header recognition, checksum calculation, header alignment, etc.
Kernel bridge does not directly interact with these features.
If you wish an ARM-based processor with on-chip L2 switching capabilities,
consider i.MX287. See i.MX28 Reference Manual, Chapter 29 and
i.MX28 EVK Linux Reference Manual, Chapter 16 for more
details.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
i.MX6UL Ethernet controllers offer certain acceleration to the OS
network stack, but these features mostly offload above-L2 tasks, such
as header recognition, checksum calculation, header alignment, etc.
Kernel bridge does not directly interact with these features.
If you wish an ARM-based processor with on-chip L2 switching capabilities,
consider i.MX287. See i.MX28 Reference Manual, Chapter 29 and
i.MX28 EVK Linux Reference Manual, Chapter 16 for more
details.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------