最近在开发imx6ul,发现LCD的工作模式是DE模式 ,不是我们常规的HV模式。LCD虽然可以显示,但是对于之前使用的VGA芯片是不能正常工作。各位大神,有谁知道如何修改LCD的模式,修改成HV模式?不胜感激!
Hi shi
in imx6 .dts file remove:
hsync-active = <0>;
vsync-active = <0>;
de-active = <1>
and set correct hsync,vsync timings in "display-timings", as for example below:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------