imx6Q 使用AR8031的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6Q 使用AR8031的问题

3,858 Views
jingyangxie
Contributor V

公司自制imx6q主板,完全参照官方imx6q-sdb主板原理图设计,现在AR8031工作不正常,网络环回没问题,但是ping不同主机,芯片发送时钟GTX_CLK和发送使能TX_EN均无输出,接收时钟为125MHZ波形,外部竞争25M正常,有遇到类似情况的吗?

ps:BSP为官方原版4.1.15

Labels (2)
0 Kudos
3 Replies

2,437 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Jingyang,

    有2个关键的时钟位置,一个是工作时钟25MHz,一个是AR8031给到CPU的ENET_REF_CLK引脚的参考时钟,这是输入给到CPU内部MAC的,这个时钟也必须要有的。

    另外,你要再仔细地核对一下AR8031的图纸和我们sabreSDB比较一下,从NVCC_ENET的MAC电源到AR8031出来的几个LDO应用,这里比较容易出错。

    最后,检查一下你的RJ45,硬件上查一下引脚的对应情况,从RJ45壳内1-8的信号线到焊盘之间,是不是正常的。

Weidong

0 Kudos

2,437 Views
jingyangxie
Contributor V

您好,现在的现象是板卡100M的速率,接交换机或或者路由器能通,换成1G就不通,如果板卡与主机直接通过网线连接的话,就完全不同(不管什么速率),这大概是什么原因引起的?

0 Kudos

2,437 Views
wtt
Contributor I

您好:

以上问题, “芯片发送时钟GTX_CLK和发送使能TX_EN均无输出” 以及“网线连接的话,就完全不同”,我也遇到了,现在无法解决,请问您是怎么解决掉的?

     谢谢!

0 Kudos