imx6DualLite bus freq issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6DualLite bus freq issue

1,566 Views
_angelo_
Contributor III

Hi,

on a module i have here, with a 1600 ddr3, imx-based kernel 4.9.184 , imx-busfreq driver moves, in certain cases, speed from 24 to 400Mhz, and completely freeze the system.

Is the jump to 400Mhz correct for a ddr3 1600 ( MT41K128M16JT-125) ? 

Was there any known bug in this driver ?

 

Thanks

Angelo

 

0 Kudos
Reply
3 Replies

1,559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Angelo

 

yes 400Mhz is correct. One can try to run ddr test with latest RPA tool and rebuild image with

new calibration coefficients found from ddr test

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/11082...

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6ULL-LPDDR2-Script-Aid/ta-p/1121785

try with nxp linux releases :

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga

 

Best regards
igor

0 Kudos
Reply

1,545 Views
_angelo_
Contributor III

Hi Igor,

thanks.

I performed calibration and stress test from u-boot by nxp tools.

Running from 327 to 672 Mhz, with or without calibration, stress test reach 620, where i start to get errors.

Also, producer of this sbc is confirm they don't see any issue. So i am still investigating.

Have still one question, in case.

Why stress test gives immediate error if i set a frequency of 24Mhz, and busfreq instead uses 24Mhz as starting idle point ?

 

Thanks

Tags (2)
0 Kudos
Reply

1,542 Views
igorpadykov
NXP Employee
NXP Employee

ddr test supports only dll on mode as described in

 

Best regards
igor

0 Kudos
Reply