imx6DL,kernel hang when excute /etc/init.d/hwclock.sh stop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6DL,kernel hang when excute /etc/init.d/hwclock.sh stop

466 Views
wushengyong
Contributor II

Our board is designed base on mx6sabresd demo, CPU is MCIMX6U7CVM08AC, the RTC on chip is not used(RTC_XTALI is grounding), the issue is that kernel hang when excute /etc/init.d/hwclock.sh stop, and the revision of CPU is as showing:

CPU:   Freescale i.MX6DL rev1.3 at 792 MHz

but this issue don't hanppen on another board with 1.2 revision CPU:

 CPU:   Freescale i.MX6DL rev1.3 at 792 MHz

what's difference between 1.2 and 1.3 version CPU about this issue?

and how to fix this issue?

Labels (1)
0 Kudos
1 Reply

403 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About the difference between 1.2 and 1.3 version you can see details in the datasheet 7 Revision History

IMX6SDLCEC.pdf https://www.nxp.com/docs/en/data-sheet/IMX6SDLCEC.pdf
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos