imx6DL怎么让kernel logo 只显示一个小企鹅并且居中显示???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6DL怎么让kernel logo 只显示一个小企鹅并且居中显示???

1,970 Views
zhaojingrongzha
Contributor I

Dear Freescale,

  目前我们的使用IMX6DL,我们项目的需求是:不在Uboot显示logo,放到kernel显示静态的boot logo,目前平台默认是左上角显示两个小企鹅,而我们的要求是在居中显示一张自定义的图片,改怎么实现???

谢谢!

Labels (2)
0 Kudos
4 Replies

1,641 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi zhaojingrong,

Which BSP and board are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,641 Views
zhaojingrongzha
Contributor I

Dear frescale,

  目前已经OK,我们还是采用freescale的补丁方案,不在kernel中显示logo,而是采用uboot中显示logo。之前想在kernel中显示logo的原因是,uboot+kernel启动的时间过长,导致android logo显示之前黑屏时间比较长。

目前我们的uboot+kernel总的时间可以优化到1.5s,而andrioid动画运行的时候大概在1.8s左右,所以这个logo显示与否不是特别重要了。

谢谢各位的解答。

0 Kudos

1,641 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi zhaojingrong,

您好,i.MX6DL是双核的,所以内核启动时候有两个企鹅。你这里想在内核启动时候显示你自己定义的图片,你要修改一下内核中logo文件,将原来的动画替换成你自己的那个。
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,641 Views
强王
Contributor IV

的你自己改代码,调坐标

最好还是你做一张和屏幕一样大的图片,这样换logo方便

0 Kudos