imx6 w/Kernel 3.0.35 for mcfg tools: Unhandled fault: Imprecise External Abort

cancel
Showing results for 
Search instead for 
Did you mean: 

imx6 w/Kernel 3.0.35 for mcfg tools: Unhandled fault: Imprecise External Abort

660 Views
jkobs2014
Contributor III

I am having a very strange failure on the 3.0.35 kernel.  We have a mostly-identical sister board that has no such fault.

Kernel Revision 3.0.35

Patches Applied (all ltib patches distributed && as many patches up to 3.0.101 as possible)

** it doesn't matter if I'm taking straight 3.0.35 ltib based code or not, no change to the failure ***

Bad Board:

Processor: imx6 solo : MC1MX6S7CVM08AB / XAA1317

DDR3: 3QK17 / D9PSL x 2

DDR3 I/O voltage @ 1.5 volts

Good Board:

Processor: imx6 solo : MC1MX6S7CVM08AB / XAA1350

DDR3: 3UK17 / D9QTF

DDR3 I/O voltage @ 1.35 volts

The failure is:

50] Unhandled fault: imprecise external abort (0x1c06) at 0xf932d7a1.

<0>[    0.092526] Internal error: : 1c06


This is happening just after the kernel attempts to do a __schedule() of the first threads in the system.  It is just after the normal kernel debug line:


"CPU: Testing write buffer coherency: ok."

but I've added debug to get further into the code

__schedule:4293 <<< extra debug to tell me the line number of where I am in __schedule()

<5>[0.092414] Scheduling: swapper <<< extra debug to tell me what thread I am about to schedule, prints out next->comm[] in task structure.


Notice that I'm capturing this from RAM after a restart: there is no serial console or debug output functioning after the kernel boots.


Any thoughts on why this might be happening?  Any and all thoughts are welcome.




0 Kudos
3 Replies

148 Views
jkobs2014
Contributor III

Just to clarify the issue a little.

First off, notes that several instances (every one we have tested) of the "bad board" board fail, and all instances (up to 10 boards) of the "bad board" have had no failure.  Essentially these are two distinct revisions of the board, with PCB changes in addition to the part changes mentioned above (NO changes to the line-lengths and layout to the DDR3).

More details of the crash:

kernel_init is a kernel thread

kernel_init is responsible for executing do_basic_setup

do_basic_setup calls do_initcalls

one of the arch_initcalls is customize_machine

customize_machine would pick the board_file and execute it.

In other words... because the device does not even run kernel_init I cannot get the board-file to execute.  which means that the problem is so fundamental, we cannot even reconfigure the board as needed.

I have seen some other references that indicate this might be some kind of u-boot failure...?

0 Kudos

148 Views
jkobs2014
Contributor III

Update:

the kernel is crashing exactly at kernel_thread_helper, at the very first instruction. the very first instruction is a

msr CPSR_c, r7

10601f80: 20637020 3c5b203a 34303038 38306131     pc : [<80041a08

0x8041a08 == kernel_thread_helper

objdump @ kernel_thread_helper

80041a08 <kernel_thread_helper>:
80041a08:       e121f007        msr     CPSR_c, r7
80041a0c:       e1a00004        mov     r0, r4
80041a10:       e1a0e006        mov     lr, r6
80041a14:       e1a0f005        mov     pc, r5

But also from the crash log:

106020e0: 616c4620 203a7367 76637a6e 52492020     Flags: nzcv  IR
106020f0: 6f207351 20206666 73514946 206e6f20    Qs off  FIQs on
10602100: 646f4d20 56532065 32335f43 53492020     Mode SVC_32  IS
10602110: 52412041 5320204d 656d6765 6b20746e    A ARM  Segment k

In other words: Mode is SVC_32, and if I understand correctly, we should be allowed to execute the msr into r7 without causing a fault.

Now.... since this is an "imprecise" abort, perhaps the crash didn't happen exactly @ 0x80041a08?

Lost and confused.

0 Kudos

148 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion? (https://community.freescale.com/docs/DOC-99909 )

Thank you for using Freescale Community.

0 Kudos