imx6 vivante GPU rotation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 vivante GPU rotation

2,481 Views
ioannisgragopou
Contributor I

Hi,

we need to rotate the display by 90o CCW in xserver environment. I searched the posts and a lot of people say that vivante_drv doesn't support rotation. If you need portrait mode in the display than you have to use fbdev driver. Is that true?

Thanks,

Ioannis

Labels (1)
0 Kudos
Reply
4 Replies

1,330 Views
gragopoulos
Contributor I

OK, thanks. I am looking forward.

0 Kudos
Reply

1,330 Views
lily_zhang
NXP Employee
NXP Employee

If you are talking about XRandR extension, it will be supported in future release.

0 Kudos
Reply

1,330 Views
EricNelson
Senior Contributor II

Do you have an ETA for this?

We're seeing some issues of tearing when using fbdev, and are trying to decide whether to dig into the details or wait.

0 Kudos
Reply

1,330 Views
gusarambula
NXP TechSupport
NXP TechSupport

Unfortunately this is true; Vivante’s driver does not support rotation as of today.

0 Kudos
Reply