imx6 usb boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
6,095件の閲覧回数
bonzo
NXP Employee
NXP Employee

Is there anyway to start uboot on a Sabre Lite board (or other board) from a USB thumb drive? 

Is this even possible?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,214件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

From the mx6 reference manual:

"The i.MX 6Series boot ROM supports the following boot devices:

NOR Flash

NAND Flash

OneNAND Flash

SD/MMC

Serial ATA (SATA) HDD

Serial ROM devices"

,so you you cannot boot directly from a USB thumb.

What you can do is to boot from one of the supported medium and then boot the kernel from a USB thumb.

Mainline U-boot does support loading a kernel from a USB thumb.

Regards,

Fabio Estevam

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,215件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

From the mx6 reference manual:

"The i.MX 6Series boot ROM supports the following boot devices:

NOR Flash

NAND Flash

OneNAND Flash

SD/MMC

Serial ATA (SATA) HDD

Serial ROM devices"

,so you you cannot boot directly from a USB thumb.

What you can do is to boot from one of the supported medium and then boot the kernel from a USB thumb.

Mainline U-boot does support loading a kernel from a USB thumb.

Regards,

Fabio Estevam

0 件の賞賛
返信
3,214件の閲覧回数
manjunathjoshi
Contributor V

Hello Fabio,

Can you just elaborate on mainline u-boot you are talking about?   I was in need of little more info on the same.

The info i mean to say is the path for the source or the download option.  Anything else that's required to know.

Regards,

Manju

0 件の賞賛
返信