imx6 uboot 2015.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 uboot 2015.04

1,136 Views
jaiganesh
Contributor III

Greetings,

Does Freescale have any plan of supporting u-boot 2015.04 officially for iMX6 (Sabresd board)?.

I have cloned the git repo for u-boot from:

         git://git.freescale.com/imx/uboot-imx.git

But I cannot find any branch with 2015.04. So, just asking if freescale have any future plan to support u-boot 2015.04?

Regards,

Jai Ganesh

Labels (2)
Tags (1)
0 Kudos
2 Replies

556 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jai

u-boot 2015.04 will be supported on next linux BSP release

planned on end of this year.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

556 Views
jaiganesh
Contributor III

Hello Igor,

Thanks. Next BSP release means, will the kernel version also be upgraded. I can see the latest kernel version Freescale working on is "3.14.38" and the yocto poky version is "fido". (I guess, both of them are in beta stage).

So, Freescale will also upgrade kernel (like 4.xx version) as well as yocto poky (1.9)?

Regards,

Jai Ganesh

0 Kudos