imx6 - u-boot binary format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 - u-boot binary format

1,330 次查看
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.


Initially we used L3.0.35_4.** release based u-boot binary.


In L3.0.35_4.** release based binary, the boot able u-boot binary is u-boot.bin.  But in  Linux 3.10.17_1.0.0-GA, the boot able u-boot binary is u-boot-imx.



We would like to know,  the difference between these two formats. Since in Linux 3.10.17_1.0.0-GA BSP also u-boot.bin is generated.


Please suggest us.


 

Thank You,

Regards,

Ansari

0 项奖励
回复
1 回复

1,005 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

please look below for answer

u-boot.bin and u-boot.imx

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复