imx6 spi read/write dma support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 spi read/write dma support

1,229件の閲覧回数
ferdi
Contributor I

Hello All:

I would ask if there is a linux3.0.35 based on SPI DMA IMX6Q transfer support, to solve the problem of SPI data overflow, other web pages have a connection with DMA SPI support but can not be opened.

Best regards!

ラベル(4)
0 件の賞賛
返信
1 返信

932件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ferdi

one can develop such driver using existing linux uart driver with sdma support, also

some suggestions are given on

How to do a SPI data transfer using SDMA on iMX6DL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信