imx6 solo +PHY KSZ9031 ping issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 solo +PHY KSZ9031 ping issue

2,845 Views
fangmingan
Contributor I

Hi all,

   After porting the latest PHY driver from Micrel, this PHY can be recognized. But we found the following issues:

1.  I have verified on two sets, ping time is too long, the average is hundreds ms on both of them(PC gigabit ethernet card connected to PHY 9031, the connecting is 1000M full and the result is as the attached picture  ). Why?

2.  I checked the MDC clock rate ,it is about  5.5MegaHz,not 2.5M?How to change it ?

  We work on android 4.0 and the kernel is 3.0

Thanks  a lot

Fangming

Labels (6)
0 Kudos
Reply
1 Reply

1,543 Views
fangmingan
Contributor I

According to the following discussion,  add "enable_wait_mode=off" in the boot params  solved this ping latency issue

i.MX6Q SabreSD Catastrophic Ethernet Latencies

I still need help  to instruct how to change the MDC clock rate.

0 Kudos
Reply