imx6 solo +PHY KSZ9031 ping issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 solo +PHY KSZ9031 ping issue

2,012 次查看
fangmingan
Contributor I

Hi all,

   After porting the latest PHY driver from Micrel, this PHY can be recognized. But we found the following issues:

1.  I have verified on two sets, ping time is too long, the average is hundreds ms on both of them(PC gigabit ethernet card connected to PHY 9031, the connecting is 1000M full and the result is as the attached picture  ). Why?

2.  I checked the MDC clock rate ,it is about  5.5MegaHz,not 2.5M?How to change it ?

  We work on android 4.0 and the kernel is 3.0

Thanks  a lot

Fangming

标签 (6)
0 项奖励
1 回复

710 次查看
fangmingan
Contributor I

According to the following discussion,  add "enable_wait_mode=off" in the boot params  solved this ping latency issue

i.MX6Q SabreSD Catastrophic Ethernet Latencies

I still need help  to instruct how to change the MDC clock rate.

0 项奖励