imx6 sabresd 3.14 kernel booting issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 sabresd 3.14 kernel booting issue.

Jump to solution
4,687 Views
narasimhuluorug
Contributor III

Hello,

I am facing the below log issue. I am unable to get login to rootfs.

Reached target Network.

[  OK  ] Started Network Name Resolution.

Console: switching to colour frame buffer device 80x30

[***   ] A start job is running for dev-ttymxc3.device (1min 18s / 1min 30s)..

[ TIME ] Timed out waiting for device dev-ttymxc3.device.

[DEPEND] Dependency failed for Serial Getty on ttymxc3.

[  OK  ] Reached target Login Prompts.

[  OK  ] Reached target Multi-User System.

Regards,

Narasimha.

1 Solution
2,413 Views
igorpadykov
NXP Employee
NXP Employee

Hi narasimhulu

reason may be wrong board configuration, as ttymxc3

is used for sabre ai boards, not sabre sd, please check

attached Release Notes Table 11. Common kernel boot parameters,

and Table 2. U-Boot configurations. Check aslo sect.5.1 Build

configurations Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
2,414 Views
igorpadykov
NXP Employee
NXP Employee

Hi narasimhulu

reason may be wrong board configuration, as ttymxc3

is used for sabre ai boards, not sabre sd, please check

attached Release Notes Table 11. Common kernel boot parameters,

and Table 2. U-Boot configurations. Check aslo sect.5.1 Build

configurations Yocto Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,413 Views
arunmench
Contributor I

Hi,

I am also facing the similar issue.

Narasimha please let me know in which config file we have enable CONFIG_FHANDLE=y , CONFIG_IKCONFIG=y?

Thanks,

Arun

0 Kudos
Reply
2,413 Views
narasimhuluorug
Contributor III

Hi Igor,

This issue i resolved by modifying the config file i.e enlbled CONFIG_FHANDLE=y , CONFIG_IKCONFIG=y.

Thanks allot.

Best Regards,

Narasimha

2,413 Views
liyigang
Contributor III

thank you narasimhuluoruganti

0 Kudos
Reply
2,413 Views
arunmench
Contributor I

for me the Getty is starting on tty1...

         Starting Bluetooth service...

[  OK  ] Started Getty on tty1.

         Starting Getty on tty1...

[  OK  ] Started Login Service.

[  OK  ] Started Bluetooth service.

[  OK  ] Started Network Service.

         Starting Hostname Service...

[  OK  ] Reached target Network.

[FAILED] Failed to start Hostname Service.

See "systemctl status systemd-hostnamed.service" for details.

random: nonblocking pool is initialized

[*     ] A start job is running for dev-ttymxc3.device

0 Kudos
Reply