imx6 reboot hangs at flush_pmd_entry

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 reboot hangs at flush_pmd_entry

ソリューションへジャンプ
3,898件の閲覧回数
agherzan
Contributor II

We have an IMX6Q platform on which we encounter a very strange issue.

While rebooting the system, platform hangs @ flush_pmd_entry(pmd). This is probably because one of the CPUs ends up crashing and won't restart. Don't have a debugger to check the actual state of the machine.

log:

root@android:/ # reboot

[   15.914484] SysRq : Emergency Remount R/O

[   15.930771] EXT4-fs (mmcblk0p6): re-mounted. Opts: (null)

[   15.949119] EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)

[   15.963710] EXT4-fs (mmcblk0p7): re-mounted. Opts: (null)

[   15.969570] Emergency Remount complete

[   16.022363] imx2-wdt imx2-wdt.0: Device shutdown: Expect reboot!

[   16.028632] Restarting system.

<HANG>

Mention: using fsl kernel 3.0.35

The exact asm line where system hangs is (tlbflush.h):

<>if (tlb_flag(TLB_DCLEAN))                                                                                                                                                                                                                 

<><-->asm("mcr<-->p15, 0, %0, c7, c10, 1<>@ flush_pmd"                                                                                                                                                                                      

<><--><-->: : "r" (pmd) : "cc");

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
2,407件の閲覧回数
agherzan
Contributor II

We found the root of the issue. It seems like activating one of these CONFIGs generated this issue:

CONFIG_ARM_ERRATA_430973=y
CONFIG_ARM_ERRATA_458693=y
CONFIG_ARM_ERRATA_460075=y
CONFIG_ARM_ERRATA_742230=y
CONFIG_ARM_ERRATA_742231=y
CONFIG_PL310_ERRATA_588369=y
CONFIG_ARM_ERRATA_720789=y
CONFIG_PL310_ERRATA_727915=y
CONFIG_ARM_ERRATA_743622=y
CONFIG_ARM_ERRATA_751472=y
CONFIG_ARM_ERRATA_794072=y
CONFIG_ARM_ERRATA_761320=y
CONFIG_ARM_ERRATA_753970=y
CONFIG_ARM_ERRATA_754322=y
CONFIG_ARM_ERRATA_754327=y

Deactivating these configs fixed this.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,408件の閲覧回数
agherzan
Contributor II

We found the root of the issue. It seems like activating one of these CONFIGs generated this issue:

CONFIG_ARM_ERRATA_430973=y
CONFIG_ARM_ERRATA_458693=y
CONFIG_ARM_ERRATA_460075=y
CONFIG_ARM_ERRATA_742230=y
CONFIG_ARM_ERRATA_742231=y
CONFIG_PL310_ERRATA_588369=y
CONFIG_ARM_ERRATA_720789=y
CONFIG_PL310_ERRATA_727915=y
CONFIG_ARM_ERRATA_743622=y
CONFIG_ARM_ERRATA_751472=y
CONFIG_ARM_ERRATA_794072=y
CONFIG_ARM_ERRATA_761320=y
CONFIG_ARM_ERRATA_753970=y
CONFIG_ARM_ERRATA_754322=y
CONFIG_ARM_ERRATA_754327=y

Deactivating these configs fixed this.

0 件の賞賛
返信
2,407件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi agherzan

what reference board you followed designing your board ?

Is it Freescale Sabre board ? On Sabre board this should not

happen because reset (Wdog output) connected to MMPF0100

PWRON (SPF-27392 rev.C3.pdf schematic), which cold reset whole

system. So all CPUs should restart healthly.

If it is not so, then this problem seems reported below

Discussing the Linux ARM kernel

Since this is common problem for arm kernels please post this issue

on that forum.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------