There is a system:IMX6 Q+2GB DDR+32GB eMMc+10.1 Inch display.
When the system runs a period of time,the screen becomes error and black ,IMX6 is crash. The debug UART outputs nothing and can not be input something.
WHY this Problem happen and how to solve it?
Hi CAI
reason may be ddr errors, so one can test memory with ddr test and
update image with new ddr calibration coefficients found from test
i.MX6/7 DDR Stress Test Tool V3.00
recommended to use nxp linux releases described on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks,igor
we have do DDR stress Test ,and it passed and update image with new ddr calibration coefficients.But the Problem still exists.
Calibration:
MR Value: 0004,
DDR Freq: 365
Stress Test:
StarFreq:200
EndFreq:528
What other way can be check?
what bsp used in the case, please try latest nxp linux releases described on
Best regards
igor
Hi,igorpadykov:
I have try to measure the imx6 32.768khz clock and 24MHZ wave.The Vp-p seems not conforming to the requirements.meet to the picture.
24MHZ:
32.768KHZ:
the requirement is below.
Hi CAI
one can check clock guidelines provided in i.MX6 System Development User’s Guide
https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf
Best regards
igor
Dear igor,
BSP used in the case is Android8.0 Linux version 4.9.17,this problem exist in this case ,but it don't exit in the other item.