imx6 mfgtool support for u-boot 2014.04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 mfgtool support for u-boot 2014.04

2,531件の閲覧回数
mohammeduddin
Contributor I

Hi

I am trying to generate a firmware u-boot for MFG (imx-3.14.28_1.0.0_ga-mfgtools) using u-boot 2014.04 version. I followed the procedure provided in the mfgtools' document to configure u-boot and kernel image for MFG which is attached in this post. I tried running the tool and dumping the images on imx6 board but it hangs in the middle of loading u-boot. The following log is shown in the mfgtool.log file:

DLL version: 2.5.1

Monday, November 09, 2015 17:18:10   Start new logging

ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[008DDBC0]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[008E09A0]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[008E6F80]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[008E9D60]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[050E2048]

ModuleID[2] LevelID[1]: new MxHidDeviceClass

ModuleID[2] LevelID[10]: new MxHidDevice[050E94A8]

ModuleID[2] LevelID[10]: Device Manager thread is running

ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop

ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0

ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is C:\Users\irfan.m\Desktop\mfgtool\L3.14.28_6UL9x9_patch_mfg-tools\mfgtools\Profiles\linux\OS Firmware\firmware\u-boot-imx6qnano_sd.imx

The tool hangs at this stage and the process won't proceed any further. Therefore, I would like to know whether u-boot 2014.04 has support for mfgtool? And if it supports, are the changes shown in the document attached enough to generate u-boot for MFG firmware? If somehow the u-boot firmware is generated sucessfully, will it support the kernel generated using 3.14.28 linux kernel version? please help.

Regards

Mohammed Irfan Uddin

ラベル(4)
0 件の賞賛
1 返信

1,124件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mohammed

please follow sect.6.2 Manufacturing Tool, MFGTool attached

Yocto Guide. Note, uboot../board/freescale/mx6sabresd/*.cfg file

(like mx6dl_4x_mt41j128.cfg) should be updated with new custom board

ddr settings obtained from DDR Tester:

i.MX6/7 DDR Stress Test Tool V2.20

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛