imx6 low power mode wakeup and reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 low power mode wakeup and reset

1,368件の閲覧回数
ilyyxfe
Contributor I

hello

my new board is using imx6sllevk , the power supply and the main peripheral component the same as MCIMX6SLL-EVK-Schematics.

i make the system sleep

when i use ttymxc0 to wake up system. sometimes it can wakeup normally, sometimes it just reset the system.

it seems that the longer time it sleep, it increased risk for reset

and uboot showed the reset cause is POR.

besides, i find some trouble.

1. i can "reboot" the system by ttymxc0 successfully,

but when i use reset button , it can not reset the system. at the same time , the ttymxc0 also can not work. the system look seemed halted. I can only reset the system by power on again.

2. next i check the reset button.

it can work during the u-boot, kernel start process. but it can not work since the login.

can you give me some advice about  how to fix it?

ラベル(3)
0 件の賞賛
返信
1 返信

1,170件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhang

one can run ddr test and rebuild image with new calibration coefficients

found from test (put them in uboot/board/freescale/mx6sllevk/imximage.cfg)

i.MX6/7 DDR Stress Test Tool V3.00 

imximage.cfg\mx6sllevk\freescale\board - uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信