imx6 linux4.1.15 X11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 linux4.1.15 X11

591 Views
jieh朱
Contributor III

Hello, I use imx6 to build the X11 file system with yocto. I use capacitive touch. When I run the X11 graphical interface, the capacitive touch can't be used normally. I am sure my touch driver is normal. How can I troubleshoot and solve
Looking forward to your reply

0 Kudos
3 Replies

452 Views
jieh朱
Contributor III

[1610026.589] (--) RandR disabled
[1610026.591] (II) AIGLX: Screen 0 is not DRI2 capable
[1610026.591] (EE) AIGLX: reverting to software rendering
[1610026.642] (II) AIGLX: enabled GLX_MESA_copy_sub_buffer
[1610026.643] (II) AIGLX: Loaded and initialized swrast
[1610026.643] (II) GLX: Initialized DRISWRAST GL provider for screen 0
[1610026.643] (II) VIVANTE(0): Setting screen physical size to 270 x 158
[1610026.791] (II) config/udev: Adding input device icn85xx_ts (/dev/input/event0)
[1610026.791] (**) icn85xx_ts: Applying InputClass "evdev pointer catchall"
[1610026.791] (II) LoadModule: "evdev"
[1610026.791] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[1610026.798] (II) Module evdev: vendor="X.Org Foundation"
[1610026.798] compiled for 1.18.0, module version = 2.10.1
[1610026.798] Module class: X.Org XInput Driver
[1610026.798] ABI class: X.Org XInput driver, version 22.1
[1610026.798] (II) Using input driver 'evdev' for 'icn85xx_ts'
[1610026.798] (**) icn85xx_ts: always reports core events
[1610026.798] (**) evdev: icn85xx_ts: Device: "/dev/input/event0"
[1610026.798] (--) evdev: icn85xx_ts: Vendor 0 Product 0
[1610026.798] (--) evdev: icn85xx_ts: Found 3 mouse buttons
[1610026.798] (--) evdev: icn85xx_ts: Found absolute axes
[1610026.798] (--) evdev: icn85xx_ts: Found x and y absolute axes
[1610026.798] (--) evdev: icn85xx_ts: Found absolute touchpad.
[1610026.798] (II) evdev: icn85xx_ts: Configuring as touchpad
[1610026.798] (**) evdev: icn85xx_ts: YAxisMapping: buttons 4 and 5
[1610026.799] (**) evdev: icn85xx_ts: EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200
[1610026.799] (**) Option "config_info" "udev:/sys/devices/virtual/input/input0/event0"
[1610026.799] (II) XINPUT: Adding extended input device "icn85xx_ts" (type: TOUCHPAD, id 6)
[1610026.799] (II) evdev: icn85xx_ts: initialized for absolute axes.
[1610026.799] (**) icn85xx_ts: (accel) keeping acceleration scheme 1
[1610026.799] (**) icn85xx_ts: (accel) acceleration profile 0
[1610026.799] (**) icn85xx_ts: (accel) acceleration factor: 2.000
[1610026.799] (**) icn85xx_ts: (accel) acceleration threshold: 4
[1610026.800] (II) config/udev: Adding input device icn85xx_ts (/dev/input/mouse0)
[1610026.800] (II) No input driver specified, ignoring this device.
[1610026.800] (II) This device may have been added with another device file

I saw my touch screen recognized as a touchpad

0 Kudos

452 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos

452 Views
jieh朱
Contributor III

Hello, thank you for your reply.
I saw my touch screen recognized as a touchpad
How can I modify it to correctly recognize it as a touch screen?

0 Kudos